4. Introduction
4.1. Purpose of this Tutorial
The purpose of this tutorial is to demonstrate how to accomplish common initial tasks. The tutorial uses the Advertiser Demo ble_adv as a starting point and
gradually shows how to implement support for the following:
Simple debugging output via UART
Modification of basic BLE configurations
Control of digital outputs
Monitoring of digital inputs
Setting a simple timer
DA14592 DEVKIT-PRO and DA14594 DEVKIT-PRO
The DA14592 DEVKIT-PRO and DA14594 DEVKIT-PRO share the same motherboard. The only difference between these two development kits lies in their respective daughterboards. What applies to the DA14592 is equally applicable to the DA14594. For clarity, this tutorial is using the DA14592 Dev Kit as an example.
4.2. How long should it take?
This tutorial requires 45-60 minutes to complete. For more information the user may consult the accompanied documentation. These are mentioned as for further reading.