Logo
  • 1. Prerequisites
  • 2. Abstract
  • 3. How DA1453x Boots from host MCU ?
  • 4. Launch e2 studio and create the RL78 application
  • 5. Application Testing
  • 6. Appendices
  • 7. Terms and Definitions
  • 8. Revision history
  • 9. Feedback and support ?
Getting started with DA14531 and FSP BLE Framework
  • R18UZ0090EE0001: Getting started with DA1453x and RL78 BLE Framework on Renesas Microcontrollers

R18UZ0090EE0001: Getting started with DA1453x and RL78 BLE Framework on Renesas Microcontrollers

contents

  • 1. Prerequisites
  • 2. Abstract
  • 3. How DA1453x Boots from host MCU ?
    • 3.1. overview
    • 3.2. boot options
    • 3.3. Setting Up the RL78/G23-128p:Fast Prototyping Board (RTK7RLG230CSN000BJ) and the DA1453x Pmod™
  • 4. Launch e2 studio and create the RL78 application
    • 4.1. create the Renesas RL78 C/C++ Project
    • 4.2. Profile development with QE for BLE
    • 4.3. QE GATT Profile
    • 4.4. Source Code Modifications
    • 4.5. Building and running the application
  • 5. Application Testing
    • 5.1. Flow of the code
    • 5.2. GTL interface
    • 5.3. BLE profile validation
    • 5.4. What Next ?
  • 6. Appendices
    • 6.1. Setting-up the logic analyzer to work with GTL
  • 7. Terms and Definitions
  • 8. Revision history
  • 9. Feedback and support ?
Next

© Copyright 2025, Renesas Electronics Corporation.