1. Prerequisites
To start building a fully working solution that allows booting from host Renesas microcontroller the following tools are being used:
- Hardware tools: - Computational workstation (e.g. PC or Laptop)
- 32-bit or 64-bit processor with 1 GHz processing speed 
- 1 GB RAM 
- 2 GB free disk space 
- Renesas EK-RA6M4 kit or any other Renesas RA microcontroller development kit. 
- USB cable for power supply and for on-board debugging. A micro USB cable is provided with the EK-RA6M4 kit. 
 
 
 
- Software tools: - Renesas Flexible Software Package v5.4.0 platform installation which includes: - e2 studio 2024-04 
- FSP 5.4.0 or later 
- GCC Arm Embedded 13.2.1 
 
 
- Bluetooth® LE explorer application
- Renesas Smartbond for IOS Use the QR code below 
- Renesas Smartbond for Android. Use the QR code below 
 
 - Figure 1 iOS Renesas SmartBond - Figure 2 Android Renesas SmartBond