11. 名词解释和定义
BLE Bluetooth Low Energy 低功耗蓝牙
COM Communication Port 通讯接口
CS Chip Select 芯片选择
DBG Debug 调试
EEPROM Electrically Erasable Programmable Memory 通电可擦除可编程存储器
FTDI Future Technology Devices International 菲迪亚特——USB接口设备公司
GPIO General Purpose Input/Output 通用型輸入輸出
HW Hardware 硬件
IDE Integrated Development Environment 集成开发环境
IRQ Interrupt Request 中断请求
LED Light Emitting Diode 发光二极管
OS Operating System 操作系统
OTP One Time Programmable 一次性可编程
PC Personal Computer 个人电脑
RF Radio frequency 射频频率
SDK Software Development Kit 软件开发套件
SoC System on Chip 片上系统
SPI Serial Peripheral Interface 串行外设接口
SRAM Static Random Access Memory 静态随机存取存储器
SW Software 软件
SWD Serial Wire Debug 串行线调试
TCK JTAG Test Clock JTAG测试时钟
TMS JTAG Test Mode Select JTAG测试模式选择
UART Universal Asynchronous Receiver/Transmitter 通用异步收发器
USB Universal Serial Bus 通用串行总线