2. Getting Started

2.1. How to Use CodeLess

The CodeLess is a quick Bluetooth® Low Energy solution that can be used out of the box without writing a single line of source code. It uses the well-known concept of AT Commands (ASCII instructions) that can be used to perform various tasks and in particular:

  • Control of Bluetooth® LE connectivity: Bluetooth® LE connect/disconnect, advertise, stop advertising, change roles (central/peripheral), scan for nearby devices, report Bluetooth® LE address, etc

  • Interaction with the environment/sensor read out: set/get GPIOs, read external interfaces, read battery, report GPIO status etc

These AT commands allow control over the local device and remote device, and easily integrate in a third-party microcontroller.

One can simply control from the Terminal and no IDE is required.

_images/noIDE.png

Figure 6 No IDE Required

The user is free to choose any third-party terminal or Renesas’s CodeLess Host application. Refer to Chapter 7 for more information and how to download the application to your local PC.

_images/terminal.png

Figure 7 CodeLess Using Terminal

Android users may want to check Renesas’s SmartConsole for an AT command execution application. Refer to Chapter 8 for more information.

_images/atscreen.png

Figure 8 SmartConsole Application

2.2. Hardware Setup

This manual explains the use of Pro-Kit to show the examples, however, you can use the basic kit as well. The setup to implement CodeLess examples for DA145xx is given below.

To quickly get started with the CodeLess on a terminal, download and execute from the SysRAM using the Booter configuration as mentioned below. To execute from SPI Flash, refer to UM-B-083 to follows steps to program the SPI Flash.

Note

  • Using the DA14531-00FXDEVKT-P motherboard, you can use either DA14531-00,DA14531-01, DA14531 Module, DA14585 or DA14586 daughterboard with the same fly-wire and jumper connections. The DA14531 USB Kit cannot be configured to boot from SPI flash and also operate a 2/4 wire UART - for this reason it is not well suited to being used as a platform for CodeLess.

  • Using the DA14535-00FXDEVKT-P motherboard, you can use either DA14531-00,DA14531-01, DA14531 Module OR DA14535 Module daughterboard with the same fly-wire and jumper connections. The DA14531 USB Kit and DA14535 USB Kit cannot be configured to boot from SPI flash and also operate a 2/4 wire UART - for this reason it is not well suited to being used as a platform for CodeLess.

Setup on DA14535-00FXDEVKT-P Motherboard

  1. Use the flywires to connect from J1[UTX] to J2[P06], J1[URX] to J2[P05], J1[URTS] to J2[P07] and J1[UCTS] to J2[P08] as shown in Figure 9.

  2. Use the jumpers to enable the SPI Flash and connect the rest of the jumpers as shown in Figure 9.

  3. Connect the Pro-DK to PC via USB cable.

  4. Two green LEDs lit up: D2, and D4.

_images/da14535_535dau.svg

Figure 9 DA14535 Setup on DA14535-00FXDEVKT-P: SPI and 4-wire UART for CodeLess Execution

Setup on DA14531-00FXDEVKT-P Motherboard

  1. Use the flywires to connect from J1[UTX] to J2[P26], J1[URX] to J2[P25], J1[URTS] to J2[P27] and J1[UCTS] to J2[P28] as shown in Figure 10.

  2. Use the jumpers to enable the SPI Flash and connect the rest of the jumpers as shown in Figure 10.

  3. Connect the Pro-DK to PC via USB cable.

  4. Three LEDs lit up: D1, D2, and D4.

_images/pro_531.png

Figure 10 DA1453x Setup on DA14531-00FXDEVKT-P: SPI and 4-wire UART for CodeLess Execution

Figure 9, Figure 10, Figure 11, and Figure 12 display also the 4-wire UART connections from the Pro-DK motherboard to DA145xx daughterboard overview.

_images/4wire.png

Figure 11 DA145xx 4-wire UART Connection Overview


The pin mapping on the DA145xx is in the following table:

Table 2 Pin Mapping

DA145XX Pin

Function

P0_6

UART TX

P0_5

UART RX

P0_7

UART RTS

P0_8

UART CTS

_images/module.png

Figure 12 DA14531 Module Setup on the DA14531-00FXDEVKT-P: 4-wire UART for CodeLess


_images/531585.png

Figure 13 DA1458x Setup on DA14531-00FXDEVKT-P: SPI and 4-wire UART for CodeLess

Setup on DA14580 Pro-DK or DA1458x Basic Kit for DA1458x

  1. Connect the three-way jumper to enable concurrent access to SPI-Flash and UART interface.

  2. Connect the Pro-Kit via USB cable to your PC.

  3. Three LEDs lit up: D1, D4, and D6.

  4. For the LED example, when using Pro-Kit, the LED D3 toggles and for Basic Kit, LED D7 toggles.

Note

The red blocks indicate where the jumpers are supposed to be placed.

_images/5315852.png

Figure 14 DA1453x Setup on DA14580 Pro-Kit

_images/setup.png

Figure 15 DA1458x Setup on Pro-Kit

_images/basicsetup.png

Figure 16 DA1458x Setup on Basic-Kit

2.3. Software Setup

The CodeLess SDK comes with the following firmware images. Depending on the SoC and application, the user can download the appropriate firmware.

Pre-compiled binaries provided with the SDK:

  • DA14531-00
    • CodeLess for DA1453x datapump: codeless_531_00_datapump.hex

    • CodeLess for DA1453x standalone SET TWO : codeless_531_00_set_two_standalone.hex

    • CodeLess for DA14531 standalone: codeless_531_00_standalone.hex

  • DA14531-01
    • codeless_531_01_datapump.hex

  • DA14535
    • codeless_535.hex

  • DA14585
    • codeless_585.hex

  • DA14586
    • codeless_586.hex

For the examples in the Manual, CodeLess for DA14531-00 standalone (SET TWO) is used. Also, depending on the application and the set of commands supported in each firmware, the user is free to choose the appropriate one. To see the list of commands supported for each target, see Section 9.

Likewise, the user can also add their custom commands by following the Chapter 6 and by compiling the code using Keil compiler.

To send your first AT command, follow the steps:

  1. Load CodeLess firmware into DA145xx using SmartSnippets™ Toolbox. Use the Booter over Serial wire debug (SWD) to download the firmware to SysRAM or use Flash Programmer to burn the firmware onto flash and execute from flash. Refer to SmartSnippets™ Toolbox User Manual Chapter 8 and 13.

  1. Open SmartSnippets™ Toolbox, select project or create a new one with any appropriate name, JTAG serial number, Target, and then click Open as shown in Figure 16.

_images/open_project.png

Figure 17 SmartSnippets Configuration

  1. Go to Tools, select Booter, browse to your firmware, and then click Download as shown in Figure 17.

_images/download_hex.png

Figure 18 Downloading to SysRAM

  1. To send AT commands, use the terminal to communicate with the board with the following settings:

    • PORT : <COM_Port>

    • BaudRate : 57600

    • DataBits : 8

    • StopBits : 1

    • Parity : None

    • Flow Control : None

    • Transmit Text: Append CR

_images/portsettings.png

Figure 19 Serial Port Settings

  1. Send your first AT command.

_images/terminal_test.png

Figure 20 AT over Terminal

Note

When the DA145xx powers up, it will stay awake for ten seconds and then go to extended sleep. If a character is received via UART within the 10 second window, the device will stay awake until it receives a sleep command (AT+SLEEP=1). Send a ‘@’ via the UART to wake up a sleeping device.

Alternatively, Renesas SmartBond™ Flash Programmer tool lets the user program a flash device for the DA1453x SoC. This is a quicker way to get things going with the CodeLess. The list of hex files are shown in the Figure 21.

_images/firmware_web.png

Figure 21 Flash Programmer Tool Download Firmware from Web

The instructions on how to use the tool is explained in the User Manual UM-B-138.


Demonstration of Renesas SmartBond™ Flash Programmer Tool


2.4. CodeLess Bluetooth Services

The CodeLess service UUID is the following: 866d3b04-e674-40dc-9c05-b7f91bec6e83. The following table lists the characteristics that the CodeLess service provides.

Table 3 CodeLess characteristics

Characteristic

UUID

Length

Properties

Comments

CodeLess Inbound Command characteristic

914f8fb9-e8cd-411d-b7d1-14594de45425

1 – 165 bytes

Read, Write

A CodeLess AT command can be written here. The read property is not used.

CodeLess Outbound Command characteristic

3bb535aa-50b2-4fbe-aa09-6b06dc59a404

1 – 165 bytes

Read, Write

The response of a previously issued AT Command can be read. The write property is not used.

CodeLess Flow Control Characteristic

e2048b39-d4f9-4a45-9f25-1856c10d5639

1 byte

Notify, read, write

A notification that data is available from Bluetooth® LE CodeLess peer.

Apart from the CodeLess service the software supports both the SUOTA service and the DSPS service.

2.5. SPI Set of Commands

Based on the underlying controller hardware, the CodeLess software supports Serial Peripheral Interface operations with a dedicated set of commands. The operations supported are SPI configuration, reading and writing of external devices with certain limitations:

  • The CodeLess Software supports only SPI master mode operation

  • Multiple slave devices are not supported

  • The SPI clock frequencies can be 2,4 and 8 MHz

For more details on the dedicated SPI set of commands refer to Chapter 9.

2.6. Event Management

The CodeLess software supports several events that can be used to indicate the state of the device to an external host. If activated, each event outputs a specific string to the serial port. Currently the following six events are supported:

  • On initialization: If the event is activated, as soon as the device is initialized, an unsolicited message will be printed to the serial port to indicate that the device is working. From this point on, the device is fully functional and AT Commands can be sent to the serial port

  • On connection: If the event is activated, as soon as a Bluetooth connection is established, the CodeLess software will send an unsolicited message to the serial port

  • On disconnection: If the event is activated, as soon as a Bluetooth connection is dropped, an unsolicited message will be sent to the serial port to indicate that the device has disconnected

  • On wakeup: If the event is activated, an unsolicited message will be sent to the serial port as soon as the device wakes up from sleep

All events are disabled, by default, on startup and the user must enable the desired events using the related event management commands that are documented in Chapter 9. The status of the events can be queried at any time.

Note

The status of the events is not retained in case of a reset or power cycle, unless non-volatile storage is activated within the source code. If non-volatile storage is activated, then the CodeLess software will try to restore the status of the events on startup. If not, any desired events must be activated again by the host. No events are printed if the Codeless software is in binary transfer mode.

2.7. Bonding Database Management

Bonding allows two connected devices to exchange and store security and identity information to create a trusted relationship. Therefore, in the future an encrypted connection can be re-established without the need to exchange encryption keys for the second time. The CodeLess software supports a bonding database that can store bonding information for several external devices. The implementation has the following characteristics:

  • The database can store bonding information for up to five different devices

  • If the database is not full and new bonding entry arrives it will be stored in one of the empty slots

  • If the database is full and new bonding information arrives, then the older bonding entry is erased. The new entry becomes the most recent entry in the database

  • Entries can be marked persistent. A persistent entry does not participate in the replacement mechanism and remains in the database regardless of new arrivals

  • If all entries are marked persistent, then no more bonding information can be stored in the database

  • If a connection is re-established using a database entry, this entry becomes the most recent one in the database

The database can be managed using a related set of AT commands. The related commands can clear the bonding database, change the persistence status of an entry, remove a selected entry and import entries from an external host. It must be noted that the bonding database is not retained on reset or on power cycle. Therefore, the database must be exported and then reimported back by the host.

2.8. Event Handlers

In addition to event management support, the CodeLess software supports the execution of AT commands on three predefined events (on connection, on disconnection and on wakeup). The user can enter a set of commands from the CodeLess command set that will be executed sequentially when the event occurs as if the user entered the commands through the console. If the handler is empty no commands will be executed.

2.9. Flow Control and Sleep Modes

Hardware flow control using UART RTS/CTS signals is possible using the AT+FLOWCONTROL command. When the device boots, it is by default not using Hardware (HW) flow control. In binary mode the HW flow control signals the available space of buffers of the device (RTS) and the availability of the host (CTS). In command mode, the RTS/CTS signals have important role in signaling their sleep mode or waking up the device or host. Flow control is tightly interconnected with sleep modes.

The host may enable or disable sleep mode of the CodeLess device using the AT+SLEEP command.

  • If HW flow control is disabled, the device may be woken from a high to low transition of UART RX signal, this can be a dummy UART byte of value 0x00

  • If HW flow control is enabled, the device’s RTS signal is deasserted. The device may be woken from a high to low transition of CTS signal

There is also a host sleep mode supported. If the host wishes to enter its own sleep mode it should inform the CodeLess device using the AT+HOSTSLP command.

  • If HW flow control is disabled, the device will wake up the host by issuing a <wkup_byte> for <wkup_retry_times> every <wkup_retry_interval>

  • If HW flow control is enabled, the device will wake up the host by toggling its RTS for <wkup_retry_times> every <wkup_retry_interval>

In both cases the host should acknowledge the wakeup by issuing an “AT” command.

Note

In Binary mode if flow control is disabled (using AT+FLOWCONTROL), the device never enters sleep mode because this will cause loss of data. If flow control is enabled the RTS signal is asserted when the device is active in connection events.

Table 2 and Table 3 provide information regarding the sleep modes with and without the HW flow control.

Table 4 Sleep Modes without RTS/CTS Flow Control

Command Format

Enter Sleep

Exit Sleep

Description

Device sleep

AT+SLEEP = 1

A dummy byte 0x00 from host.

This does not suspend every function of the device; it enables extended sleep. The device will acknowledge exiting sleep mode by an AWAKE string.

Host sleep

AT+HOSTSLP = 1,0, 100, 1000

By issuing byte 0x00.

The byte that will be issued is the second parameter of AT+HOSTSLP. The host should acknowledge exiting sleep mode with an AT command.



Table 5 Sleep Modes with RTS/CTS Flow Control

Command Format

Enter Sleep

Exit Sleep

Description

Device sleep

AT+SLEEP = 1

A High to low of CTS signal (input to the device).

This does not suspend every function of the CodeLess device, it enables extended sleep. The RTS will be deasserted. The device will acknowledge exiting sleep mode by an AWAKE string and will assert RTS.

Host sleep

AT+HOSTSLP = 1,0, 100, 1000

A High to low of RTS signal (input to the host).

The second parameter of AT+HOSTSLP is not effective. The host should acknowledge exiting sleep mode with an AT command.