1. Introduction to CodeLess

1.1. Before You Start

  • Download the latest CodeLess SDK from the Codeless reference page and SmartSnippets™ Toolbox from the SmartBond™ Development Tools web page.

  • The Codeless SW package content section in the Appendix Section 11 describes the SDK directory structure, gives explanation about folders and their content

  • Download any local Terminal, such as TeraTerm, Termite, or any other you are familiar with

  • Arrange for a temperature sensor for performing some examples described in the following chapters. We use Adafruit MCP9808 I2C Temperature sensor, the Thermo 8 Click board™ from MIKROE could be also used.

  • Make sure the USB driver is installed correctly and the properties of the USB driver look similar to Figure 1. Go to Device Manager, right-click the correct USB serial port, and click Properties > General. Otherwise, you can install FTDI driver from http://www.ftdichip.com/Drivers/VCP.htm.

Application 1

Figure 1 Correctly Installed USB Driver

1.2. CodeLess Objectives

Important

Document Updates for v6.380.18.63 Release

The latest features and enhancements introduced in the recent codeless v6.380.18.63 release are detailed below:

  • Migrating CodeLess to the latest SDK (6.0.20.1338).

  • Additional target has been added supporting the DA14535 IC.

  • The Arm GCC compiler along with SmartSnippets Studio® can be used to build and run the CodeLess reference design.

Note

e2 studio support To start building a fully working solution on e2 studio and Codeless you can refer to the e² studio SDK 6 Getting Started Guide.

The CodeLess development allows you to quickly get started with wireless IoT applications with a set of AT Commands:

  • Currently supports our DA1453x/DA1458x SoCs

  • Enabling control of hardware interfaces as well as Bluetooth® Smart via simple AT command interface

  • Control of the local as well as remote peer device with a single command set

  • Completely configurable hardware setup. No SW development required

  • Great for sensor evaluation (I2C or Analog input port)

  • Can be easily expanded

  • Both central and peripheral role supported in one firmware

  • Available as source code, hex, and binary files as well as header file for implementation into an external microcontroller

  • Can be integrated easily in a 3rd party Microcontroller

Table 1 presents the differentiation among the variants of the DA14531-0x.

Table 1 DA14531-0x Product Variants Differentiation

BLE Features

DA14531-00

DA14531-01

DA14535

LE Central support

YES

NO

YES

LE Observer support

YES

NO

YES

support the LL Privacy feature (privacy on the controller side)

YES

NO

NO

Compatible with SDK 6.0.12 or higher

YES

NO

NO

Compatible with SDK 6.0.18

YES

YES

NO

Compatible with SDK 6.0.22 or higher

YES

YES

YES

Rest of features

YES

YES

YES

Note

  • The DA14530 is pin-for-pin compatible with the DA14531 and provides cost savings by operating from an internal LDO, eliminating the cost of a DC/DC inductor.

Note

  • The SmartBond™ DA14586 is a SoC with an integrated Flash (2 Mbit). The DA14586 is pin-to-pin compatible with the DA14585

1.3. Highlighting Features

Besides a basic set of AT commands to read and control Bluetooth® LE functions and interface configuration, CodeLess support the following features:

  • Implements a dedicated mode to exchange seamlessly binary data between devices

  • Supports several additional AT commands (Bluetooth® LE and interfaces configuration, security, signal indication, PWM etc)

  • Configurable to execute a set of existing commands when certain events occur (on connection, on disconnection, on wake-up etc)

  • Has over the air firmware update capabilities (SUOTA)

  • Fully manages the bonding database (import/export entries, clear database, set persistency etc.)

  • Supports various Bluetooth® LE security scenarios (ranging from secure connections to no security at all)

  • Supports sleep mode scenarios

  • Works with SPI command interface in addition to UART/remote Bluetooth® LE device

  • Supports non–volatile storage for selected commands

  • Host support: Graphical user interface written in Python/mobile phone application

1.4. Overview of the User Manual

  • Implementation of CodeLess examples to get an idea of its vast application capabilities and ease of use

  • Implementation of Binary mode

  • Use of SmartConsole Android application

  • Use of Renesas’s Codeless Host application

  • The examples that will be covered are:

    • Toggle LED on local board

    • Read ADC on local board

    • Write/Read I2C (using I2C Temperature sensor) on local board

    • Advertise/Scan/connect to the remote board

    • Toggle LED on remote board

    • Read ADC on remote board

    • Write/Read I2C on remote board

CodeLess can be used for more applications than are mentioned above. Typical applications are:

  1. UART to UART wireless connection: CodeLess can be controlled from a PC or a 3rd party microcontroller.

Application 1

Figure 2 UART to UART Wireless Connection

Warning

The DA14531-01 can’t be configured as a central, to run this demo you should consider the DA14531-00.

  1. Remote access of Peripheral from the Central: The IO control, sensors, and analog signals connected on the peripheral device can be remotely accessed from the Central device.

Application 2

Figure 3 Remote Access of Peripheral from the Central

Warning

The DA14531-01 can’t be configured as a central, to run this demo you should consider the DA14531-00.

  1. CodeLess for debugging: Local connection to the CodeLess for debugging and evaluation of sensor or other connected hardware is easily implemented.

Application 3

Figure 4 CodeLess for Debugging


  1. Smartphone control of the peripheral.

Application 4

Figure 5 Smartphone Control of the Peripheral


1.5. Where is it Applicable?

  • Simplest Bluetooth® LE product implementation

  • Accelerating time to market for Simple Bluetooth® LE pipe applications connected to an external MCU

  • Rapid prototyping and Proof of Concept

  • Sensor evaluation

  • Renesas’s platform evaluation and introduction to SDK

  • Platform for further development

  • Hardware debugging