1. Abstract
This guide is intended to help customers setup the hardware development environment, install required software, download, and run an example application on DA14585/586 Pro Development Kit platform.
Warning
The current revision of this guide (4.1) covers only the DA14585 and DA14586 devices. The DA148580, DA14581 and DA14583 devices are beyond the scope of this document.
2. Prerequisites
To start evaluation or project development on Renesas DA14585/6 product sets – the following tools are recommended.
- Hardware tools:
- Computational workstation (e.g. PC or Laptop)
32-bit or 64-bit processor with 1 GHz processing speed
1 GB RAM
2 GB free disk space
DA14585/586 Pro Development kit as a Mother-board
DA14585/6 Daughter-board
USB cable to power supply Pro Development kit and perform on-board debugging
- Software tools:
- Windows™ Operating System (e.g Windows 10)
Terminal software such as RealTerm, Putty or Tera Term. This document uses Tera Term for its examples.
SmartSnippets™ Studio 2.0.8 or later which can be installed on Windows, see Section Section 6.
Software Development Kit (SDK) latest version of SDK6 for project development
Note
When installing SmartSnippets™, all the sub-component drivers and software tools needed for DA14585/6 development will be installed.