2. SmartBoot Image Creation Tool

DA14533 device

For DA14533 device, pins P06, P09 and P011 are not available.

SmartBoot Image Creation Tool




SUotA Only


Include a bootable two-wire UART boot step in the boot-loader:


Enable an initiation pin for SUOTA_only during reset or power-cycle:


Optionally, drop an application firmware file here

.img file with image headers only. See additional information.

Only .img files are allowed.



filename.bin ❌


Log: