1. Abstract
This guide is intended to help customers setup getting started with the DA14531 TINY™ Bluetooth Module.
The DA14531 TINY™ Module, is the first Renesas Bluetooth® Low Energy module based on world’s lowest power DA14531 SoC.
2. Prerequisites
- To start the evaluation or project development on Renesas DA14531 product sets, the following tools are being used here however the process is same with other development kit:
- Hardware tools:
Computational workstation (e.g. PC or Laptop)
32-bit or 64-bit processor with 1 GHz processing speed
1 GB RAM
2 GB free disk space
DA14531-00FXDEVKT-P as a Motherboard
DA14531-0x TINY™ Module FCGQNFN 24 Package (DA14531-00/DA14531-01- QFN daughterboard).
USB cable for power supply to the Pro Development kit and for on-board debugging
- Software tools:
Terminal software such as RealTerm, Putty or Tera Term. This document uses Tera Term for its examples
SmartSnippets™ Toolbox or later, which can be installed on Windows.
Hint
When SmartSnippets™ is installed, all the sub-component drivers and software tools needed for DA14531 development are also installed.
- Bluetooth® explorer tool:
Type chrome://bluetooth-internals/#devices into the address field of the Chrome Browser to use the built-in tool (PC with Win10 or MAC book)
Renesas Smartbond for IOS Use the QR code below
Renesas Smartbond for Android. Use the QR code below
Renesas SmartBond for iOS:
Figure 1 Scan the QR Code to Install Renesas SmartBond for iOS
Renesas SmartBond for Android:
Figure 2 Scan the QR Code to Install Renesas SmartBond for Android