3. Introduction
The DA14531 SmartBond TINY™ Module is a Renesas Bluetooth® Low Energy module based on the ultra-low power DA14531 SoC. The module offers a unique combination of the lowest power and the integration of all external components including antenna at a very affordable price. The module is designed to enable the use of Bluetooth® Low Energy in applications where Bluetooth® Low Energy could not be used until now because of cost or complexity. The bigger picture is to drive Bluetooth® Low Energy technology into every application, turning every product into a connected IoT node to drive the next 1 billion IoT devices in the market. The combination of an affordable price, the lowest power consumption and ease of use makes the DA14531 TINY™ Module an ideal product for the mass market, including the makers community.
- Ordering Information (Production):
Table 1 Part Information Table Part Number
Size (mm)
Shipment Form
Pack Quantity
DA14531MOD-00F0100
12.5 x 14.5 x 2.8
Reel
1 Kpcs
The development kit includes a set of hardware (development board with an on-board debugger) and is supported by a Software Development Kit SDK6 (that is, a development toolchain, source code examples, and so on), and documentation.
3.1. Guide Purpose
The purpose of this guide is to provide an overview of DA14531 module and describe the setup of the hardware and installation of the software tools to fully use the module.
The guide is organized as follows:
Section Section 4 describes the hardware components and their initial installation and setup.
Sections Section 5 and Section 6 describe the installation of the SmartSnippets™ DA1453x SDK software, along with all necessary tools.
Section Section 7 contains all steps for downloading and executing your first DA1453x Application.
3.2. How long should it take?
This tutorial requires 10-15 minutes to complete. For more information the user may consult the accompanied documentation, these are mentioned as for further reading.
3.3. Unboxing the package content
The DA14531 Pro Development Kit box can be ordered via various distributors. The DA14531 Development box contains the following items:
DA14531 DEVKIT-P Motherboard
Bluetooth low energy Module (DA14531MOD-00F0100)