6.6. BLE Coexistence with other 2.4GHz radios
The aim of this chapter is to describe the main steps to enable WLAN coexistence support for the DA1453x/DA1458x.
6.6.1. Introduction
Figure 92 WLAN coexistence with BLE
The WLAN coexistence feature on DA1453x/DA1458x is designed to allow multiple 2.4 GHz devices to operate without signals from one radio interfering with adjacent radios. This is done by a handshaking protocol between the BLE device and the other 2.4 GHz device using the following signals:
- WLAN_COEX_BLE_EIP signal
The DA1453x/DA1458x can communicate its radio status in advance using the abovementioned signal. WLAN_COEX_BLE_EIP is an envelop of the scheduled TX and RX radio activity of the BLE Radio and it starts before the actual radio activity so it can upfront inform the coexisting system of scheduled RF activity. The signal is de-asserted synchronously directly after radio activity is finished.
- WLAN_COEX_BLE_PRIO signal
The DA1453x/DA1458x can enable a priority line to indicate that it can not be interrupted for a defined activity. The activity for which BLE needs priority can be defined through the API.
The WLAN_COEX_BLE_PRIO signal is controlled internally by the DA1453x/DA1458x firmware, following certain user configurable rules. In the following table are listed all available priorities.
Table 109 The commands to configure the priorities for the WLAN coexistence feature Rule
Command
Priority Type
1
wlan_coex_prio_criteria_add(BLEMPRIO_SCAN, LLD_ADV_HDL, 0);
Active scan
2
wlan_coex_prio_criteria_add(BLEMPRIO_ADV, LLD_ADV_HDL, 0);
Advertise
3
wlan_coex_prio_criteria_add(BLEMPRIO_CONREQ, LLD_ADV_HDL, 0);
Connection request
4
wlan_coex_prio_criteria_add(BLEMPRIO_LLCP, 0, 0);
Control packet
5
wlan_coex_prio_criteria_add(BLEMPRIO_DATA, 0, 0);
Data packet
6
wlan_coex_prio_criteria_add(BLEMPRIO_MISSED, 0, 4);
Missed events (in this example, after 4 bad packets)
- WLAN_COEX_24G_EIP signal
Input signal to DA1453x/DA1458x device. External 2.4GHz device event in progress indication.
Note
Detailed information about WLAN Coexistence driver can be found in API documentation.
6.6.2. Enabling WLAN Coexistence feature
As an example, we will proceed to outline how WLAN coexistence feature could be enabled in prox_reporter_ext project:
As an example, in
da1458x_config_advanced.h, use the following preprocessor definitions in order to enable WLAN coexistence mode with or without debugging signals and set the preferred polarity of the BLE event in progress signal:
/****************************************************************************************************************/
/* WLAN coexistence mode: Enable/disable the mode. */
/****************************************************************************************************************/
#define CFG_COEX
/****************************************************************************************************************/
/* WLAN coexistence mode: Enable/disable the debugging signals. */
/****************************************************************************************************************/
#define CFG_WLAN_COEX_DEBUG
/****************************************************************************************************************/
/* WLAN coexistence mode: Controls the polarity of the BLE event in progress signal. */
/* - defined: BLE event in progress signal is active low. */
/* - undefined: BLE event in progress signal is active high. */
/****************************************************************************************************************/
#undef CFG_WLAN_COEX_BLE_EVENT_INV
The following source file must be added to the project:
wlan_coex.ccomprise the WLAN coexistence feature implementation and reside in<sdk_root_directory>\sdk\platform\driver\wifi. The files can easily be added by right click on the corresponding folder and select theAdd Existing files to Group…option.
The following include path must be added to the project. Click on the
Options for Target…and then in the C/C++ tab. In the include Paths field add the wifi folder that holds the wlan_coex.h file.
Figure 93 WLAN COEX include path
In
user_periph_setup.hthe following block of definitions should be added for WLAN coexistence pin mapping:
/****************************************************************************************/
/* WLAN COEX pin configuration */
/****************************************************************************************/
#if (WLAN_COEX_ENABLED)
#if defined (__DA14531__)
/// Input signal to device: 2.4GHz external device event in progress indication.
#define WLAN_COEX_24G_EIP_PORT GPIO_PORT_0
#define WLAN_COEX_24G_EIP_PIN GPIO_PIN_5
/// Output signal from device: BLE event in progress indication.
#define WLAN_COEX_BLE_EIP_PORT GPIO_PORT_0
#define WLAN_COEX_BLE_EIP_PIN GPIO_PIN_6
/// Output signal from device: BLE priority indication.
#define WLAN_COEX_BLE_PRIO_PORT GPIO_PORT_0
#define WLAN_COEX_BLE_PRIO_PIN GPIO_PIN_7
#if defined (CFG_WLAN_COEX_DEBUG)
/// BLE radio overruled signal pin definition.
/// This signal goes high when the BLE radio is forced to be off due to external 2.4GHz device activity.
#define WLAN_COEX_DEBUG_A_PORT GPIO_PORT_0
#define WLAN_COEX_DEBUG_A_PIN GPIO_PIN_9
/// External 2.4GHz device EIP handler signal pin definition.
/// This signal indicates when an external 2.4GHz device wants to start or stop sending data.
#define WLAN_COEX_DEBUG_B_PORT GPIO_PORT_0
#define WLAN_COEX_DEBUG_B_PIN GPIO_PIN_8
#endif
#else
/// Input signal to device: 2.4GHz external device event in progress indication.
#define WLAN_COEX_24G_EIP_PORT GPIO_PORT_0
#define WLAN_COEX_24G_EIP_PIN GPIO_PIN_0
/// Output signal from device: BLE event in progress indication.
#define WLAN_COEX_BLE_EIP_PORT GPIO_PORT_0
#define WLAN_COEX_BLE_EIP_PIN GPIO_PIN_3
/// Output signal from device: BLE priority indication.
#define WLAN_COEX_BLE_PRIO_PORT GPIO_PORT_0
#define WLAN_COEX_BLE_PRIO_PIN GPIO_PIN_2
#if defined (CFG_WLAN_COEX_DEBUG)
/// BLE radio overruled signal pin definition.
// This signal goes high when the BLE radio is forced to be off due to external 2.4GHz device activity.
#define WLAN_COEX_DEBUG_A_PORT GPIO_PORT_0
#define WLAN_COEX_DEBUG_A_PIN GPIO_PIN_1
/// External 2.4GHz device EIP handler signal pin definition.
/// This signal indicates when an external 2.4GHz device wants to start or stop sending data.
#define WLAN_COEX_DEBUG_B_PORT GPIO_PORT_1
#define WLAN_COEX_DEBUG_B_PIN GPIO_PIN_3
#endif
#endif
// GPIO IRQ number. Interrupt is fired when 2.4GHz external device event in progress signal is activated.
#define WLAN_COEX_IRQ 4
#endif // WLAN_COEX_ENABLED
In user_periph_setup.c make the following changes in order to enable properly WLAN coexistence feature:
Add the required include file. Include
wlan_coex.hin the Include Files section.
#if (WLAN_COEX_ENABLED)
#include "wlan_coex.h"
#endif
Add the following global variable definition (configuration struct for WLAN coexistence):
#if (WLAN_COEX_ENABLED)
// Configuration struct for WLAN coexistence
const wlan_coex_cfg_t wlan_coex_cfg = {
.ext_24g_eip_port = WLAN_COEX_24G_EIP_PORT,
.ext_24g_eip_pin = WLAN_COEX_24G_EIP_PIN,
.ble_eip_port = WLAN_COEX_BLE_EIP_PORT,
.ble_eip_pin = WLAN_COEX_BLE_EIP_PIN,
.ble_prio_port = WLAN_COEX_BLE_PRIO_PORT,
.ble_prio_pin = WLAN_COEX_BLE_PRIO_PIN,
#if defined (CFG_WLAN_COEX_DEBUG)
.debug_a_port = WLAN_COEX_DEBUG_A_PORT,
.debug_a_pin = WLAN_COEX_DEBUG_A_PIN,
.debug_b_port = WLAN_COEX_DEBUG_B_PORT,
.debug_b_pin = WLAN_COEX_DEBUG_B_PIN,
#endif
.irq = WLAN_COEX_IRQ,
};
#endif
Reserve GPIOs used by the module by adding the following block of code inside
GPIO_reservations()function:
#if (WLAN_COEX_ENABLED)
RESERVE_GPIO(COEX_EIP, wlan_coex_cfg.ble_eip_port, wlan_coex_cfg.ble_eip_pin, PID_GPIO);
RESERVE_GPIO(COEX_PRIO, wlan_coex_cfg.ble_prio_port, wlan_coex_cfg.ble_prio_pin, PID_GPIO);
RESERVE_GPIO(COEX_REQ, wlan_coex_cfg.ext_24g_eip_port, wlan_coex_cfg.ext_24g_eip_pin, PID_GPIO);
#if defined (CFG_WLAN_COEX_DEBUG)
RESERVE_GPIO(DEBUGPIN1, wlan_coex_cfg.debug_b_port, wlan_coex_cfg.debug_b_pin, PID_GPIO);
RESERVE_GPIO(DEBUGPIN2, wlan_coex_cfg.debug_a_port, wlan_coex_cfg.debug_a_pin, PID_GPIO);
#endif
Figure 94 Changes in GPIO_reservations() function
Call
wlan_coex_gpio_cfg()function at the end ofset_pad_functions()to initialize GPIOs used by the module and to configure 2.4GHz external device event in progress signal to act as a GPIO interrupt.
#if (WLAN_COEX_ENABLED)
wlan_coex_gpio_cfg();
#endif
Figure 95 Changes in set_pad_functions()
Last but not least, it should be mentioned that the following changes are required in
user_proxr.cin order to initialize the WLAN-BLE coexistence mode and set the BLE priority over the WLAN module.Add the required include files. Include
wlan_coex.handlld.hin the Include Files section.
#if (WLAN_COEX_ENABLED)
#include "wlan_coex.h"
#include "lld.h"
#endif
Call inside
user_on_init()the following functions:wlan_coex_init()in order to initialize the WLAN-BLE coexistence mode;wlan_coex_prio_criteria_add()function to configure the rules for the WLAN coexistence feature.
#if (WLAN_COEX_ENABLED)
wlan_coex_init();
// Adds priority case for a specific connection
wlan_coex_prio_criteria_add(WLAN_COEX_BLE_PRIO_ADV, LLD_ADV_HDL, 0);
#endif
Finally call
wlan_coex_going_to_sleep()function insideuser_validate_sleep()in order to prepare WLAN COEX mode for going to sleep.
#if (WLAN_COEX_ENABLED)
wlan_coex_going_to_sleep();
#endif
Figure 96 Changes in user_proxr.c file