8. Secure Storage
8.1. overview
Starting from SDK version 6.0.24, we introduced two app modules:
Encryption module: provides an easy-to-use API for encryption functions.
Storage module: provides an easy-to-use API for memory storage functions.
These modules are used in the bond database system to securely store encrypted bonding data.You can see how these modules work in the ble_app_security demo available in: projects\target_apps\ble_examples\ble_app_security, where sample user data is securely written to and read from flash memory.
8.2. Testing Storage and Encryption (from SDK 6.0.24)
below are the steps for Storage and Encryption tests:
1/ Initial Flash Verification:
Download the firmware using Keil or burn it to flash.
Run the device with sleep enabled and empty flash.
Use SST (Smart Snippet Toolbox) to check flash:
At offset
0x01E000, size0x294At offset
0x01F000, size0x24
The data at these locations should not be all zeros, as they are stored encrypted.
2/ Bonding and Adding User Data:
Download the firmware again using Keil.
Bond with the device using a generic BLE app.
Write
0x01to the custom profile’s control point once to add an entry to the user database.
3/ Verify Flash Contents:
Use SST to read the flash.
New bonding and user data entries should appear below the initial encrypted data.
You can identify them using the struct’s start/end headers and size.
4/ Reconnection Test:
Re-download the firmware and reconnect with the previously bonded device.
Pairing should not occur again.
Read the ADC value to confirm that the user data was properly recovered.
5/ Repeat Bond/Delete Cycle:
Disconnect and delete the bond from the phone.
Reconnect, bond again, and write
0x01to the custom profile.Repeat verification steps above.
Reconnect again to ensure data loads correctly.
6/ Storage Limit Testing:
When bonding data size is
0x1000, the 7th bond/delete cycle will exceed storage.All old entries are erased, only the last one is kept.
The same applies to the user database, which holds up to 3 entries due to smaller size.
7/ Non-Encrypted Mode:
All the above tests were also repeated with encryption disabled:
Set
BDB_ENCRYPTEDandUDDB_ENCRYPTEDto false.