1. Introduction¶
1.1. Overview¶
The key goals of this tutorial are to:
- Provide a basic understanding of implementing a custom test function in Dialogs PLT software and in particular a custom function to test the NTC connections.
- Detail all the necessary steps to implement and run the test:
- Add the code to the PLT application
- Rebuild the PLT application, add necessary hardware (resistors and/or NTC) to verify the custom test.
1.2. Production Line Tool (PLT)¶
Dialog is offering a production test and programming unit that enables you to reduce the time to Ramp-up at a lower cost.
The Production Line Tool (PLT) helps to increase throughput in volume test & programming of units centered around the Dialog Bluetooth® IC’s.
Features
- Ease of integration: DLL based commands
- Flexibility in programming OTP/Flash/EEPROM
- Low overall cost of tester equipment
- High level of parallelization and short testing time.
- Add customized tests
- Up to 16 times parallel programming and test
The latest release of the Production Line Tool now also supports the new devices in the SmartBond™ Bluetooth family: DA1469x and DA14531.
More information can be found on the Dialog Semiconductor support portal.
1.3. Getting started¶
Before you start you need to:
- Install the latest SmartSnippets Studio
- Download the latest SDK (DA1469x SDK10.0.8.105)
- Download the latest PLT software
These can be downloaded from the Dialog Semiconductor support portal.
Additionally, for this tutorial a Pro Development kit can be used.
Initial setup information can be found in the Getting started guide.