7. Code Overview
This section provides the code blocks needed to successfully execute this tutorial.
7.1. Advertising Task Code
In main.c file, replace the ble_adv_demo_task() application task with the following code:
/* Initialize the BLE structure related to BD address value. */
static const own_address_t user_bd_address = {
.addr_type = PRIVATE_STATIC_ADDRESS,
.addr = {0x01, 0x02, 0x03, 0x04, 0x05, 0xC0},
};
static void ble_adv_demo_task(void *pvParameters)
{
int8_t wdog_id;
gap_adv_chnl_t channel_map = GAP_ADV_CHANNEL_37;
// Remove compiler warnings about the unused parameter
( void ) pvParameters;
/* Register ble_adv_demo task to be monitored by watchdog */
wdog_id = sys_watchdog_register(false);
// Start BLE module as a peripheral device
ble_peripheral_start();
// Set device name
ble_gap_device_name_set("Renesas TTT Demo", ATT_PERM_READ);
// Set BD address to the preferred value
ble_gap_address_set(&user_bd_address, 0x00FF);
// Set advertising interval
ble_gap_adv_intv_set(min,max);
ble_gap_adv_chnl_map_set(channel_map);
// Set advertising data
ble_gap_adv_data_set(sizeof(adv_data), adv_data, 0, NULL);
// Start advertising
ble_gap_adv_start(GAP_CONN_MODE_UNDIRECTED);
for (;;) {
ble_evt_hdr_t *hdr;
/* Notify watchdog on each loop */
sys_watchdog_notify(wdog_id);
/* Suspend watchdog while blocking on ble_get_event() */
sys_watchdog_suspend(wdog_id);
/*
* Wait for a BLE event - this task will block
* indefinitely until something is received.
*/
hdr = ble_get_event(true);
/* Resume watchdog */
sys_watchdog_notify_and_resume(wdog_id);
if (!hdr) {
continue;
}
switch (hdr->evt_code) {
case BLE_EVT_GAP_CONNECTED:
handle_evt_gap_connected((ble_evt_gap_connected_t *) hdr);
break;
case BLE_EVT_GAP_DISCONNECTED:
handle_evt_gap_disconnected((ble_evt_gap_disconnected_t *) hdr);
break;
case BLE_EVT_GAP_PAIR_REQ:
handle_evt_gap_pair_req((ble_evt_gap_pair_req_t *) hdr);
break;
default:
ble_handle_event_default(hdr);
break;
}
// Free event buffer
OS_FREE(hdr);
}
}
In main.c file, replace the handle_evt_gap_connected() routine with the following code used for triggering the Update Parameter process upon a
connection event.
/* Connection index */
static uint16_t connection_index;
/* Advertising interval mode */
#define FAST_ADV_INTERVAL (0)
#if (FAST_ADV_INTERVAL == 1)
static const uint16_t min = BLE_ADV_INTERVAL_FROM_MS(80); // 80 ms
static const uint16_t max = BLE_ADV_INTERVAL_FROM_MS(100); // 100 ms
#else
static const uint16_t min = BLE_ADV_INTERVAL_FROM_MS(1000); // 1000 ms
static const uint16_t max = BLE_ADV_INTERVAL_FROM_MS(1500); // 1500 ms
#endif
/* Update connection parameters. */
static void conn_param_update(uint16_t conn_idx)
{
gap_conn_params_t cp;
cp.interval_min = defaultBLE_PPCP_INTERVAL_MIN;
cp.interval_max = defaultBLE_PPCP_INTERVAL_MAX;
cp.slave_latency = defaultBLE_PPCP_SLAVE_LATENCY;
cp.sup_timeout = defaultBLE_PPCP_SUP_TIMEOUT;
ble_gap_conn_param_update(conn_idx, &cp);
}
/*
* This timer callback notifies the task that time for discovery, bonding and
* encryption elapsed. Connection parameters can be changed.
*/
static void conn_param_timer_cb(OS_TIMER timer)
{
/* Call the function which is responsible for the connection parameters update. */
conn_param_update(connection_index);
}
static void handle_evt_gap_connected(ble_evt_gap_connected_t *evt)
{
/*
* Manage behavior upon connection
*/
connection_index = evt->conn_idx;
/* When the timer expires connection parameters will be re-negotiated */
OS_TIMER update_timer = OS_TIMER_CREATE("conn_timer", OS_MS_2_TICKS(5000),
OS_TIMER_FAIL, (uint32_t) OS_GET_CURRENT_TASK(),
conn_param_timer_cb);
OS_TIMER_START(update_timer, OS_TIMER_FOREVER);
}
Optionally, in main.c file change the advertising data:
/*
* BLE adv demo advertising data
*/
static const uint8_t adv_data[] = {
#if dg_configSUOTA_SUPPORT
0x03, GAP_DATA_TYPE_UUID16_LIST_INC, 0xF5, 0xFE,
#endif
0x14, GAP_DATA_TYPE_LOCAL_NAME,
'H', 'o', 'w', ' ', 'A', 'r', 'e', ' ', 'Y', 'o', 'u', ' ', 'T', 'o', 'd', 'a', 'y', ' ', '?'
};
7.2. Macro Definitions
In customer_config_eflash.h file, add the following macro definitions:
/* Peripheral-specific configurations */
#define defaultBLE_PPCP_INTERVAL_MIN (BLE_CONN_INTERVAL_FROM_MS(500)) // 500 ms
#define defaultBLE_PPCP_INTERVAL_MAX (BLE_CONN_INTERVAL_FROM_MS(750)) // 750 ms
#define defaultBLE_PPCP_SLAVE_LATENCY (0) // 0 events
#define defaultBLE_PPCP_SUP_TIMEOUT (BLE_SUPERVISION_TMO_FROM_MS(6000)) // 6000 ms