1. Abstract
This guide is intended to help customers understand the basic Bluetooth® Low Energy Adverstising concept and how it is implemented in the DA1459x SDK.
Example code is provided.
Note
DA1459x is referring to DA14592 and DA14594.
The below table presents the various members of the DA1459x product family and their supported features.
Features |
DA14592 |
DA14594 |
|---|---|---|
RAM capacity |
96 kB |
96 kB |
eFlash capacity |
256 kB |
256 kB |
Bluetooth® LE 5.2 core features |
YES |
YES |
Bluetooth® LE 5.3 core features |
NO |
YES |
Advertising Extensions support |
NO |
YES |
Periodic Advertising support |
NO |
YES |
AoA/ AoD support |
NO |
YES |
Wireless Ranging (WiRa) support |
NO |
YES |
Up to 32 GPIOs |
YES |
YES |
Packages |
WLCSP39 and FCQFN52 |
WLCSP39 and FCQFN52 |