1. Prerequisites
To start building a fully working solution that allows booting from host Renesas microcontroller the following tools are being used:
Hardware tools:
Computational workstation (e.g. PC or Laptop)
32-bit or 64-bit processor with 1 GHz processing speed
1 GB RAM
2 GB free disk space
CK-RX65N: Renesas Cloud Kit Based on RX65N MCU or any other Renesas RX microcontroller development kit.
USB cable for power supply and for on-board debugging. A micro USB cable is provided with the CK-RX65N kit.
Software tools:
e2 studio 2024-01 which includes support for RX MCU.
Bluetooth® LE explorer application
Renesas Smartbond for iOS Use the QR code below
Renesas Smartbond for Android. Use the QR code below
Figure 1 iOS Renesas SmartBond
Figure 2 Android Renesas SmartBond