8. Appendices
8.1. Setting-up the logic analyzer to work with GTL
Saleae plugin for Renesas GTL can be found in this GitHub repo. To Set-up the logic analyzer to work with GTL you need to follow the following steps:
Add the extension from the Marketplace
Figure 60 GTL extension
Add GTL decode analyzers
Figure 61 GTL decode
Configure the analyzer for Async Serial
Figure 62 Configure GTL analyzer