3. Introduction

The DA14535 is an ultra-low-power System-on-Chip (SoC) that combines a 2.4 GHz transceiver with an Arm® Cortex®-M0+ microcontroller. This versatile SoC serves dual roles, acting as a data pump in hosted systems or a standalone application processor.

One of its key features is the Low IQ Buck/Boost DCDC (DC-DC Converter), which operates efficiently during sleep mode, especially when in Buck mode. This allows the DA14535 to achieve exceptional ultra-low power consumption. Whether used in hosted systems or as a standalone processor, the integrated Low IQ Buck/Boost DCDC ensures outstanding energy efficiency and performance, making it a top choice for various applications.

This device is available in a small footprint while still offering large flexibility in configuration of the on-chip interfaces, making it suitable for a wide range of applications. For more information, see

DA14535 Datasheet.

The development kit comprises essential hardware, including a development board equipped with an on-board debugger. It is complemented by comprehensive support from a Software Development Kit (SDK). This SDK includes a complete development toolchain, a rich collection of source code examples, and comprehensive documentation. Together, these resources provide developers with everything they need to kick-start their projects effectively and efficiently.

3.1. Guide Purpose

The purpose of this guide is to provide an overview of the DA14535 Pro Development Kit Board and descriptions of hardware setup and installing software tools to fully use the board.

The guide is organized as follows:

  • Section 4 describes the hardware components and their initial installation and setup

  • Section 5 and Section 6 describe the installation of the SmartSnippets™ DA145xx SDK software, and other prerequisite tools

  • Section 7 contains all steps to download and execute your first DA14535 application.

3.2. How long does it take to finish the tutorial?

It will take you 30 to 40 minutes to complete this training. For more information, see the accompanying documentation. In this guide, it is customary to reference related documentation with the text for more information.

3.3. Unboxing the Package Content

The DA14535 Pro Development Kit box can be ordered via various distributors. The DA14535 Development box contains the following items:

  • DA1453x DEVKIT-P motherboard

  • Bluetooth® low energy daughterboard (DA14535-00FXDB-P)

  • Power measurement module

  • Mini USB cable.