1. Abstract
This guide serves as a comprehensive resource designed to assist customers in establishing the hardware development environment, installing necessary software components, and successfully running an example application on the DA14535 DEVKIT-P platform.
In pursuit of these objectives, the subsequent table will meticulously outline the key distinctions among the various members of the DA1453x family, providing insights for your development endeavors.
Features |
DA14531-00 |
DA14531-01 |
DA14530 |
DA14535 |
|---|---|---|---|---|
RAM |
48 kB |
48 kB |
48 kB |
64 kB |
OTP |
32 kB |
32 kB |
32 kB |
12 kB |
ROM |
144 kB |
144 kB |
144 kB |
160 kB |
Processor |
16 MHz 32-bit Arm® Cortex-M0+ |
16 MHz 32-bit Arm® Cortex-M0+ |
16 MHz 32-bit Arm® Cortex-M0+ |
16 MHz 32-bit Arm® Cortex-M0+ |
GPIOs |
6 (WLCSP17) 12 (FCGQFN24) |
6 (WLCSP17) 12 (FCGQFN24) |
12 |
12 |
Bluetooth version |
5.1 |
5.1 |
5.1 |
5.3 |
DCDC converter |
YES |
YES |
NO |
YES |
BLE firmware include L2CAP |
YES |
YES |
YES |
YES |
LE Central support |
YES |
NO |
Yes |
YES |
LE Observer support |
YES |
NO |
Yes |
YES |
Support the LL Privacy feature (privacy on the controller side) |
YES |
YES |
NO |
YES |
Compatible with SDK 6.0.10 or lower |
NO |
NO |
NO |
NO |
Compatible with SDK 6.0.12/14/16 |
YES |
NO |
NO |
NO |
Compatible with SDK 6.0.18 |
YES |
YES |
YES |
NO |
Compatible with SDK 6.0.22 or higher |
YES |
YES |
YES |
YES |