Abstract

This tutorial describes how to migrate an existing SDK 6 Keil® µVision IDE project to e2 studio. This process also migrates the project from Keil® GNU C Compiler toolchain to LLVM Embedded Toolchain for Arm®.

Note

  • This document is applicable to SDK6 version 6.0.22 and later. (DA14585/6 and DA1453x)

  • DA1453x is referring to DA14531-00, DA14531-01, DA14530 and DA14535.

  • DA1458x is referring to DA14585 and DA14586.