SPI with DMA cannot be used Rx/Tx FIFO
ID: COBALTSDK-970
Status: Open
First reported: 10.2.4.44
Fixed in: TBD
Description
When using the hardware SPI interface in combination with the DMA, it is not possible to use a FIFO level different from 0. Otherwise there is a risk to loose data during SPI transactions.
Workaround
When configuring the SPI adapter driver in combination with the DMA, make sure the fields rx_tl and tx_tl are set to 0.