4. DA1468x
4.1. Tutorials
- The key goals of this tutorial are to:
Provide a basic understanding of the Advertising Concept
Explain how to change the advertising contents and connection parameters with respect to Dialog SDK
Verify the correct functionality of the Bluetooth low energy device using the SmartSnippets Toolbox (integrated in the SmartSnippets Studio)
- The key goals of this tutorial are to:
Provide a basic understanding of the secure boot mechanism
Set up a working demonstration of firmware digitally signed and securely executed
Explain the various options the security boot toolbox has to offer
- The key goals of this tutorial are to provide:
A basic understanding of Generic ATT profile
A basic understanding of Dialog Bluetooth framework architecture
A basic understanding of Bluetooth database creation process
A complete sample project demonstrating the creation of a custom Bluetooth service
- The key goals of this tutorial are to:
Provide a basic understanding of debugging and debuggers
Explain reasons that may cause the device to fail and the steps that need to be followed depending on the root cause of the failure
Give tips and insights for dealing with failures of the system
- The key goals of this tutorial are to:
Provide a basic understanding of the external interruption mechanism
Set up a working demonstration handling an external interruption and taking action
Trigger an OS task execution based on the collected external interruption
- The key goals of this tutorial are to:
Provide a basic understanding of Adapters concept
Explain the different settings of Flash Adapters
Give a complete sample project demonstrating the usage of Flash Adapters
- The key goals of this tutorial are to:
Provide a basic understanding of adapters concept
Explain the different APIs and configurations of GPADC adapters
Give a complete sample project demonstrating the usage of GPADC and battery adapters
- The key goals of this tutorial are to:
Provide a basic understanding of adapters concept
Explain the different APIs and configurations of I2C peripheral adapters
Give a complete sample project demonstrating the usage of I2C peripheral adapters
- The key goals of this tutorial are to:
Provide a basic understanding of RTC functionality
Explain the different APIs and configurations of the RTC mechanism
Give a complete sample project demonstrating the usage of the RTC mechanism
- The key goals of this tutorial are to:
Provide a basic understanding of Adapters concept
Explain the different APIs and configurations of SPI peripheral Adapters
Give a complete sample project demonstrating the usage of SPI peripheral Adapters
- The key goals of this tutorial are to:
Start working with a customized project
Analyze the key points of the code structure
Prepare both hardware and software to run a demonstration code example
4.2. Application Notes
This guide is intended to help customers setup the hardware development environment, install required software and download and run an example application on the DA1468x development platform.
This document describes the booting sequence for all supported serial interfaces and provides the developer with the necessary information for realizing the protocol required for establishing communication between an external device and the DA1468x
Minimal reference schematic, circuit explanation and design guidelines for BLE applications based on the DA14680-01, DA14681-01, DA14682-00 and the DA14683-00 SoCs
This Application Note describes the features and usage of the Ozone Debugger, SEGGER’s source-level debugger for embedded systems.
Guidelines for designing printed antennas for 2.4 GHz Bluetooth® low energy applications on singlelayer and multi-layer PCB stack-ups
This application note explains how to setup RF testing for the DA1468x BLE SoC using various BT testers
This document describes the battery charging operation for a lithium-ion or lithium-polymer battery using the DA1468x device.
(v4.2) This document describes the DA1458x/DA1468x Production Line Tool (PLT). The various software applications, as well as the PLT hardware are explained in detail. The purpose of this document is to help users to become familiar with the tool and help them use it in a short amount of time.
(v4.3) This document describes the DA1458x/DA1468x Production Line Tool (PLT). The various software applications, as well as the PLT hardware are explained in detail. The purpose of this document is to help users to become familiar with the tool and help them use it in a short amount of time.
This document should be used as a reference guide to gain a deeper understanding of the SmartSnippets Software Development Kit (SDK). As such it covers a broad range of topics including a brief introduction to Bluetooth Low Energy (BLE), Operating System (OS) related material and a number of sections containing a more detailed technical analysis of hardware elements, for instance clock and power management
This is a guide explaining the porting from DA14681 to DA14683 silicon version.