1. DA145xx
1.1. Tutorials
Specified for DA14531 & DA14530
This document presents an overview of supported Flash devices for the DA1453x and DA14585 Bluetooth IC’s.Complete tutorial for DA14531-DA14530 and DA1458x from unboxing to configuration and more
tutorial to provide a quick introduction to the Renesas SmartBond™ SDK6, while simultaneously demonstrating how to implement some basic functionality.
overview for the DA145xx System on Chip (SoC) family of integrated circuit (IC) devices
DSPS provides a simple substitute for RS-232 connections, which includes the familiar software flow control logic via Bluetooth® Low Energy (LE).
The goal of this tutorial is not to cover every detail related to advertising
This tutorial will give an overview on how to configure DA14531 SoC (System on Chip) in one of the three available sleep modes
describes the changes and the steps needed to port an application that has been developed with DA14585/DA14586 SDK 6.0.10 release, to the latest DA1453X SDK 6.0.18 release
The Dialog SmartBond™ Flash Programmer tool lets the user program a flash device for the DA1453x, DA14585/586 and DA1469x SoCs (System on Chip)
describes how to upgrade the firmware in the Renesas US159-DA14531EVZ pmod
The goal of this tutorial is not to cover every detail related to debugging
SDK6 Known Limitations
This tutorial will give a basic understanding of Bluetooth Low Energy (BLE) security
- In this tutorial we will cover the following points
What is a server? What is a client in GATT protocol?
Basic understanding of Generic ATT profile
What is a Profile, a Custom Profile, a Custom Service and a Custom Characteristic definition
GATT custom profile application message flow
Basic understanding of custom database creation process
Add a characteristic in the custom service database
This tutorial aims to provide an introduction to using the DA145xx Peripheral Drivers that are provided as part of the Dialog Semiconductor SmartBond™ SDK6
SUOTA demonstration
shows how software updates over Bluetooth can be added to a microcontroller
- Implementation of CodeLess examples to get an idea of its vast application capabilities and ease of use
Implementation of Binary mode
Use of SmartConsole Android application
Use of Dialog’s Codeless Host application
- The examples that will be covered are:
Toggle LED on local board
Read ADC on local board
Write/Read I2C (using I2C Temperature sensor) on local board
Advertise/Scan/connect to the remote board
Toggle LED on remote board
Read ADC on remote board
Write/Read I2C on remote board
Design Examples files to help customers develop their PCB
1.2. Application Notes
This document serves as a guideline for preparing schematics and PCB layouts for your application using DA14585/DA14586.
This document presents an overview of supported Flash devices for the DA1453x and DA14585 Bluetooth IC’s
This Application Note describes how to use an external memory (I2C EEPROM or SPI Flash) with the DA14585/586. The main differences between the internal OTP and an external memory are also presented.
This tutorial shows the concept and provides guidelines step by step How to squeeze down the RAM size to 32KB and 48KB for the DA14585/586 product
Explains how to set up RF testing modes
provides the minimal reference schematic, circuit explanation, and design guidelines for BLE applications based on the DA1453x SoCs
presents an overview of supported Flash devices for the DA1453x and DA14585 Bluetooth IC’s
describes the hardware and software setup using the DA145xx-pro 376-18-B development kit for available booting options using serial interfaces such as I2C, UART, SPI and how to program a firmware into Flash, EEPROM or OTP memory
Guidelines for designing printed antennas for 2.4 GHz Bluetooth® low energy applications on singlelayer and multi-layer PCB stack-ups
contains guidelines for implementing a RFIO filter to reduce conducted and radiated spurious emissions in Bluetooth low energy applications using Dialog’s DA14531 System-on-Chip
The DA1458x Bluetooth Smart device in a WLCSP package shows sensitivity to direct sunlight and light from halogen lamps. Fluorescent tubes and UV lamps do not affect the chip’s operation. Infrared lamps have the same effect on the DA1458x WLCSP device as halogen lamps. Various methods for blocking light are discussed: coatings, molding compounds and light blocking tapes. This is applicable to the following devices in WLCSP: DA14580, DA14581, DA14585