7. QSPI Driver Example
This chapter contains the code of the Adesto AT25SL321 QSPI Flash Driver, the modifications on automode.c as well as the modifications performed on the custom_config files and the XML configuration entry. This code will not compile as is in earlier versions of the SDK than version SDK10.0.8.105.
7.1. Adesto At25SL321 Flash Driver header files
Adesto AT25SL321 Driver Header:
/**
 * \addtogroup PLA_BSP_SYSTEM
 * \{
 * \addtogroup PLA_MEMORY
 *
 * \{
 */
/**
 ****************************************************************************************
 *
 * @file qspi_at25sl321.h
 *
 * @brief Driver for flash ADESTO AT25SL321
 *
 * Copyright (C) 2016-2020 Dialog Semiconductor.
 * This computer program includes Confidential, Proprietary Information
 * of Dialog Semiconductor. All Rights Reserved.
 *
 ****************************************************************************************
 */
/**************************************** flash_configurations.xml ENTRY *****************************************
  <configuration name="Adesto AT25SL321">
    <flash_size>0x400000</flash_size>
    <flash_burstcmda_reg_value>0xa8a000eb</flash_burstcmda_reg_value>
    <flash_burstcmdb_reg_value>0x00000066</flash_burstcmdb_reg_value>
    <flash_write_config_command>0x31 0x02 0x07</flash_write_config_command>
  </configuration>
 *****************************************************************************************************************/
#ifndef _QSPI_ADESTO_AT25SL321_H_
#define _QSPI_ADESTO_AT25SL321_H_
#include "qspi_common.h"
/************************************************* JEDEC ID INFO *************************************************/
/**
 * \brief The Flash type JEDEC ID
 *
 * This is the first byte returned by the 0x9F command
 */
#define ADESTO_ID                                       0x1F
/**
 * \brief The Flash type JEDEC ID
 *
 * This is the second byte returned by the 0x9F command
 */
#define AT25SL_TYPE                                     0x42
/**
 * \brief The Flash density JEDEC ID
 *
 * This is the third byte returned by the 0x9F command
 */
#define AT25SL321_SIZE                                  0x16
/**************************************************** TIMINGS ****************************************************/
/* Flash power up/down timings in usec */
#define AT25SL321_POWER_DOWN_DELAY_US                   3 /* cannot have less than 3us delay */
#define AT25SL321_RELEASE_POWER_DOWN_DELAY_US           3 /* cannot have less than 3us delay */
#define AT25SL321_POWER_UP_DELAY_US                     10000
/************************************************ Opcodes SECTION ************************************************/
/* Status Register Opcodes */
#define AT25SL321_READ_STATUS_REGISTER_2_OPCODE         0x35
#define AT25SL321_WRITE_STATUS_REGISTER_2_OPCODE        0x31
/* Suspend/Resume Opcodes */
#define AT25SL321_ERASE_PROGRAM_SUSPEND_OPCODE          0x75
#define AT25SL321_ERASE_PROGRAM_RESUME_OPCODE           0x7A
/* Quad Read Opcode */
#define AT25SL321_FAST_READ_QUAD_OPCODE                 0xEB
/* Quad Page Program */
#define AT25SL321_QUAD_PAGE_PROGRAM_OPCODE              0x33
/********************************************** DRIVER GENERIC INFO **********************************************/
/* Quad Enable Bit Position - Status Register 2 */
#define AT25SL321_SR_2_QE_BIT_POS                       (1)
#define AT25SL321_SR_2_QE_MASK                          (1 << AT25SL321_SR_2_QE_BIT_POS)
/* Erase/Program Suspend Bit Position - Status Register 2 */
#define AT25SL321_SR_2_ESUS_BIT_POS                     (7)
#define AT25SL321_SR_2_ESUS_MASK                        (1 << AT25SL321_SR_2_ESUS_BIT_POS)
/* Extra/Mode Byte used for entering continuous read mode */
#define AT25SL321_EXTRA_BYTE_M7_M0                      0xA0
/************************************************* uCode SECTION *************************************************/
/*
 * This section is OBSOLETE in DA1469x Family products however it is maintained here for reference reasons as
 * this part is mandatory for DA14683 products.
 */
#if (dg_configFLASH_POWER_OFF == 1)
/**
 * \brief uCode for handling the QSPI FLASH activation from power off.
 */
const uint32_t at25sl321_ucode_wakeup[] = {
        0x11000001 | (((uint16_t)(AT25SL321_POWER_UP_DELAY_US*1000/62.5) & 0xFFFF) << 8),
        0xFFFF0000,
};
#elif (dg_configFLASH_POWER_DOWN == 1)
/**
 * \brief uCode for handling the QSPI FLASH release from power-down.
 */
const uint32_t at25sl321_ucode_wakeup[] = {
        0xAB000009 | (((uint16_t)(AT25SL321_RELEASE_POWER_DOWN_DELAY_US*1000/62.5) & 0xFFFF) << 8),
};
#else
/**
 * \brief uCode for handling the QSPI FLASH exit from the "Continuous Read Mode".
 */
const uint32_t at25sl321_ucode_wakeup[] = {
        0xFF000025,
        0x00FFFFFF,
};
const uint32_t at25sl321_ucode_wakeup_32bit_addressing[] = {
        0xFF000045,
        0xFFFFFFFF,
        0x00FFFFFF,
};
#endif
/********************************************** FUNCTION PROTOTYPES **********************************************/
/**
 * \brief Set the Quad Enable Bit of the Status Register if it is not already set.
 *
 * \param[in] id QSPI controller id
 */
__RETAINED_CODE static void flash_at25sl321_enable_quad_mode(HW_QSPIC_ID id);
/**
 * \brief This function returns the dummy bytes required when utilizing Fast Read Quad.
 *
 * \param[in] id QSPI controller id
 *
 * \note This function will return the number of dummy bytes required while Fast Read Quad is activated. In some QSPI Flash devices,
 *       it is possible that the number of dummy bytes required can vary depending on the operating speed.
 */
__RETAINED_CODE static uint8_t flash_at25sl321_get_dummy_bytes(HW_QSPIC_ID id);
/**
 * \brief Initialize AT25SL321 QSPI Flash
 *
 * \param[in] id QSPI controller id
 *
 * \note This function will perform all the required actions in order for AT25SL321 QSPI Flash to
 *       be properly initialized.
 */
__RETAINED_CODE static void flash_at25sl321_initialize(HW_QSPIC_ID id);
/**
 * \brief This function returns true if an erase or program operation is already suspended.
 *
 * \param[in] id QSPI controller id
 *
 * \note This function reads the status register and checks the erase/program suspend bit. If it is set then it return true since
 *       a program or erase operation is currently suspended.
 */
__RETAINED_CODE static bool flash_at25sl321_is_suspended(HW_QSPIC_ID id);
/**
 * \brief Read the Status Register 2 of the Flash
 *
 * \param[in] id QSPI controller id
 *
 * \return uint8_t The value of the Status Register 2 of the Flash.
 */
__RETAINED_CODE static uint8_t flash_at25sl321_read_status_register_2(HW_QSPIC_ID id);
/**
 * \brief Hook function called when the clock is changed
 *
 * \param[in] id QSPI controller id
 *
 * \note This function will be called prior to switching from one clock source to another. This function allows doing all
 *       the required tasks before the clock source is switched. Typical use could be setting up the proper QSPI divider
 *       to ensure that the device will continue to operate even after the clock source will be switched. E.g. Flash that supports
 *       up to 80 MHz operating speed will need to have a divider of 2 if PLL96 is picked as the source.
 */
__RETAINED_CODE static void flash_at25sl321_sys_clock_cfg(HW_QSPIC_ID id, sys_clk_t sys_clk);
/**
 * \brief Write the Status Register 2 of the Flash
 *
 * \param[in] id QSPI controller id
 * \param[in] value The value to be written.
 *
 * \note This function blocks until the Flash has processed the command. No verification that the
 *        value has been actually written is done though. It is up to the caller to decide whether
 *        such verification is needed or not and execute it on its own.
 */
__RETAINED_CODE static void flash_at25sl321_write_status_register_2(HW_QSPIC_ID id, uint8_t value);
/************************************************* CONFIG OBJECT *************************************************/
/**
 * \brief This struct configures the system for the specific flash
 *
 * \note This struct MUST be const for this to work. Therefore, assignments must
 *       not change (must be read-only)
 */
static const qspi_flash_config_t flash_at25sl321_config = {
        /* JEDEC Bytes 9Fh */
        .manufacturer_id                  = ADESTO_ID,
        .device_type                      = AT25SL_TYPE,
        .device_density                   = AT25SL321_SIZE,
        /* Flash Info */
        .memory_size                      = MEMORY_SIZE_32Mb,
        .address_size                     = HW_QSPI_ADDR_SIZE_24,
        .is_ram                           = false,
        .qpi_mode                         = false,
        /* Callbacks */
        .is_suspended                     = flash_at25sl321_is_suspended,
        .initialize                       = flash_at25sl321_initialize,
        .sys_clk_cfg                      = flash_at25sl321_sys_clock_cfg,
        .get_dummy_bytes                  = flash_at25sl321_get_dummy_bytes,
        /* Read */
        .fast_read_opcode                 = AT25SL321_FAST_READ_QUAD_OPCODE,
        .send_once                        = 1,
        .extra_byte                       = AT25SL321_EXTRA_BYTE_M7_M0,
        .break_seq_size                   = HW_QSPI_BREAK_SEQ_SIZE_1B,
        /* Page Program */
        .page_program_opcode              = AT25SL321_QUAD_PAGE_PROGRAM_OPCODE,
        .quad_page_program_address        = true,
        /* Sector Erase */
        .erase_opcode                     = CMD_SECTOR_ERASE,
        .read_erase_progress_opcode       = CMD_READ_STATUS_REGISTER,
        .erase_in_progress_bit            = FLASH_STATUS_BUSY_BIT,
        .erase_in_progress_bit_high_level = true,
        /* Program/Erase Suspend/Resume */
        .erase_suspend_opcode             = AT25SL321_ERASE_PROGRAM_SUSPEND_OPCODE,
        .erase_resume_opcode              = AT25SL321_ERASE_PROGRAM_RESUME_OPCODE,
        /* Timings */
        .power_down_delay                 = AT25SL321_POWER_DOWN_DELAY_US,
        .release_power_down_delay         = AT25SL321_RELEASE_POWER_DOWN_DELAY_US,
        .power_up_delay                   = AT25SL321_POWER_UP_DELAY_US,
};
/********************************************* FUNCTION  DEFINITIONS *********************************************/
__RETAINED_CODE static void flash_at25sl321_enable_quad_mode(HW_QSPIC_ID id)
{
        uint8_t status;
        status = flash_at25sl321_read_status_register_2(id);
        if (!(status & AT25SL321_SR_2_QE_MASK))
        {
                flash_write_enable(id);
                flash_at25sl321_write_status_register_2(id, status | AT25SL321_SR_2_QE_MASK);
        }
}
__RETAINED_CODE static uint8_t flash_at25sl321_get_dummy_bytes(HW_QSPIC_ID id)
{
        /* 2 Dummy Bytes are required for non QPI mode of operation regardless of Operating Frequency for AT25SL321. */
        return 2;
}
__RETAINED_CODE static void flash_at25sl321_initialize(HW_QSPIC_ID id)
{
        /* Set QE Bit if it is not set */
        flash_at25sl321_enable_quad_mode(id);
}
__RETAINED_CODE static bool flash_at25sl321_is_suspended(HW_QSPIC_ID id)
{
        __DBG_QSPI_VOLATILE__ uint8_t status;
        status = flash_at25sl321_read_status_register_2(id);
        return ((status & AT25SL321_SR_2_ESUS_MASK) != 0);
}
__RETAINED_CODE static uint8_t flash_at25sl321_read_status_register_2(HW_QSPIC_ID id)
{
        __DBG_QSPI_VOLATILE__ uint8_t status;
        uint8_t cmd[] = { AT25SL321_READ_STATUS_REGISTER_2_OPCODE };
        flash_transact(id, cmd, 1, &status, 1);
        return status;
}
__RETAINED_CODE static void flash_at25sl321_sys_clock_cfg(HW_QSPIC_ID id, sys_clk_t sys_clk)
{
        /* Operating Frequency larger than 96 MHz achieved through PLL so there is no need to use a divider. Empty hook function */
}
__RETAINED_CODE static void flash_at25sl321_write_status_register_2(HW_QSPIC_ID id, uint8_t value)
{
        uint8_t cmd[2] = { AT25SL321_WRITE_STATUS_REGISTER_2_OPCODE, value };
        flash_write(id, cmd, 2);
        /* Wait for the Flash to process the command */
        while (flash_is_busy(id));
}
#endif /* _QSPI_ADESTO_AT25SL321_H_ */
/**
 * \}
 * \}
 */
7.2. Modifications to automode.c
Under folder {SDK_root}/sdk/bsp/memory/src, resides source file qspi_automode.c. Find the following section…
#if (FLASH_AUTODETECT == 1)
#               include "qspi_gd25le32.h"
#               include "qspi_mx25u3235.h"
#               include "qspi_w25q32fw.h"
#               include "psram_aps1604jsq.h"
#               include "psram_aps3204jsq.h"
#               include "psram_aps6404jsq.h"
static const qspi_flash_config_t* flash_config_table[] = {
                &flash_gd25le32_config,
                &flash_mx25u3235_config,
                &flash_w25q32fw_config,
                &psram_aps1604jsq_config,
                &psram_aps3204jsq_config,
                &psram_aps6404jsq_config,
};
… and replace it with …
#if (FLASH_AUTODETECT == 1)
#               include "qspi_at25sl321.h"
#               include "qspi_gd25le32.h"
#               include "qspi_mx25u3235.h"
#               include "qspi_w25q32fw.h"
#               include "psram_aps1604jsq.h"
#               include "psram_aps3204jsq.h"
#               include "psram_aps6404jsq.h"
static const qspi_flash_config_t* flash_config_table[] = {
                &flash_at25sl321_config,
                &flash_gd25le32_config,
                &flash_mx25u3235_config,
                &flash_w25q32fw_config,
                &psram_aps1604jsq_config,
                &psram_aps3204jsq_config,
                &psram_aps6404jsq_config,
};
… to make Adesto AT25SL321 QSPI Flash discoverable through FLASH_AUTODETECT.
7.3. The custom_config_ files
In custom_config_ variant files of any custom Firmware add the following lines:
#define dg_configFLASH_AUTODETECT               (0)
#define dg_configFLASH_HEADER_FILE              "qspi_at25sl321.h"
#define dg_configFLASH_CONFIG                   flash_at25sl321_config
The above snippet disables device autodetect, defines which driver should be used and defines the name of the configuration object to be used as it is defined in the driver file.
7.4. XML Configuration Entry
Under folder {SDK_root}/utilities/python_scripts/qspi find and edit file flash_configurations.xml. Add the following entry:
<configuration name="Adesto AT25SL321">
   <flash_size>0x400000</flash_size>
   <flash_burstcmda_reg_value>0xa8a000eb</flash_burstcmda_reg_value>
   <flash_burstcmdb_reg_value>0x00000066</flash_burstcmdb_reg_value>
   <flash_write_config_command>0x31 0x02 0x07</flash_write_config_command>
</configuration>
Now, if program_qspi_config is chosen from External Tools drop-down menu, there should be a QSPI Flash Option called Adesto AT25SL321 which will set the correct values to the Product Header of any custom Firmware targetting this particular QSPI Flash Device.