3. Changing Advertising Parameters¶
This section describes how to change the advertising parameters. It covers all the necessary key elements related to advertising, specifically dealing with advertising data and intervals. It also describes the advertising channel map and mode.
3.1. Advertising Data¶
Step #1 Change the contents of the existing adv_data[ ] variable for the required advertising data.
Code snippet:
/*Bluetooth low energy adv demo advertising data*/
static const uint8_t adv_data[] = {
0x14, GAP_DATA_TYPE_LOCAL_NAME,
'H', 'o', 'w', ' ', 'A', 'r', 'e', ' ', 'Y', 'o', 'u', ' ', 'T', 'o', 'd', 'a', 'y', ' ', '?'
};
Note
The first element of the array is the size of the data to be sent plus an extra null character, that is, 19 + 1 = 20 elements or 0x14 in hexademical format. If the wrong value is given, it is likely that Bluetooth low energy device will not advertise at all so care must be taken when calculating this value.
3.2. Advertising Interval¶
Step #2 The advertising interval is the period for which a Bluetooth low energy peripheral device advertises. For this scenario we have adapted two different time slots - one in a high-speed mode and another at a lower speed. To switch between them, set the preferred mode to “1”.
Code snippet:
/* Depending on the advertising interval mode, the corresponding code segment is selected */
#if (FAST_ADV_INTERVAL == 1)
static const uint16_t min = BLE_ADV_INTERVAL_FROM_MS(80);
static const uint16_t max = BLE_ADV_INTERVAL_FROM_MS(100);
#else
static const uint16_t min = BLE_ADV_INTERVAL_FROM_MS(1000);
static const uint16_t max = BLE_ADV_INTERVAL_FROM_MS(1500);
#endif
MACRO |
Value |
Description |
|---|---|---|
FAST_ADV_INTERVAL |
0x0 |
Fast advertising mode. |
POWER_ADV_INTERVAL |
0x1 |
Slow advertising mode. Use this mode for a reduced power consuption. |
Step #3 Call the corresponding GAP function to set the min-max advertising intervals (before starting advertising and after starting the Bluetooth low energy module as a peripheral device).
Code snippet:
/*Set advertising interval*/
ble_gap_adv_intv_set(min,max);
3.3. Advertising Channel Map¶
Step #4 The channel defined in the Bluetooth Core Specification consists of 37 data communication channels and 3 advertising channels used for device discovery. The latter are allocated in different parts of the spectrum to prevent interference from concurrent activities in the ISM Band. Specifically a Bluetooth low energy device can advertise on channels 37, 38, and 39 which correspond to frequencies of 2.402 MHz, 2.2426 MHz, and 2.480 MHz respectively. SmartBond™ devices advertise successively in all enabled channels. By default, all channels are enabled. To force the Bluetooth low energy device to use only one channel, for example channel 37, use the following GAP function:
Code snippet:
/* Set advertising channel map */
gap_adv_chnl_t channel_map = GAP_ADV_CHANNEL_37;
ble_gap_adv_chnl_map_set(channel_map);
Enumeration Name |
Value |
Description |
|---|---|---|
GAP_ADV_CHANNEL_37 |
0x00 |
Select channel 37 for advertising |
GAP_ADV_CHANNEL_38 |
0x02 |
Select channel 38 for advertising |
GAP_ADV_CHANNEL_39 |
0x04 |
Select channel 39 for advertising |
3.4. Advertising Mode¶
Step #5 The advertising mode is customizable by changing the input parameter of the
ble_gap_adv_start() function. The default mode in this application is depicted in the following code snippet
and forces the Bluetooth low energy module to advertise toward all devices in the outside world.
Code snippet:
/* Start advertising */
ble_gap_adv_start(GAP_CONN_MODE_UNDIRECTED);
Enumeration Name |
Value |
Description |
|---|---|---|
GAP_CONN_MODE_NON_CON |
0x00 |
The Bluetooth low energy device advertises without permitting a connection to another central device. |
GAP_CONN_MODE_UNDIRECTED |
0x01 |
The Bluetooth low energy device advertises towards all devices regardless of their BD value. |
GAP_CONN_MODE_DIRECTED |
0x02 |
The Bluetooth low energy device advertises towards a device with a specific BD address. |
GAP_CONN_MODE_DIRECTED_LDC |
0x03 |
The Bluetooth low energy device advertises towards a device with a specific BD address using Low Duty Cycle. |