2. Prerequisites

To start the evaluation or project development on Renesas DA14531 product sets, the following tools are being used here however the process is same with other development kit:

  • Hardware tools:
    • Computational workstation (for example, PC or Laptop)

    • 32-bit or 64-bit processor with 1 GHz processing speed

    • 1 GB RAM

    • 2 GB free disk space

    • DA14531-00FXDEVKT-P as a motherboard

    • DA14531-0x daughterboard FCGQNFN 24 package (DA14531-00/DA14531-01- QFN daughterboard).

    • USB cable for power supply to the Pro Development kit and for on-board debugging

Hint

When SmartSnippets™ is installed, all the sub-component drivers and software tools needed for DA14531 development are also installed.

  • Bluetooth® explorer tool:
    • Type chrome://bluetooth-internals/#devices into the address field of the Chrome Browser to use the built-in tool (PC with Win10 or MAC book) or scan the QR code below based on your operating system

    • Renesas Smartbond for IOS:

      Use the QR code below

    ../_images/apple-store-smartbond.svg

    Figure 1 Scan the QR Code to install Renesas SmartBond for iOS

    Or

    ../_images/play-store-smartbond.svg

    Figure 2 Scan the QR Code to install Renesas SmartBond for Android