10. SPS Performance
To measure SPS performance, throughput tests have been done for the DA14531, DA14535 and the DA14585 chipsets. The UART baudrate was set to 921600 bits/s in all tests. The connection interval is 25 msec and MTU negotiated to 247, but for iPhone tests MTU=185 bytes). For the test the following hosts were used: DA1453x, DA1458x, iPhone X (iOS 13) , Samsung M33 ( Android 12) and Huawei P40 (Android 10). The SPS performance analysis gives the following results regarding the service’s throughput.
Device |
Host |
|||
|---|---|---|---|---|
DA14531 |
DA14531 |
iPhone XR |
Samsung A52S |
One Plus 7Pro |
Tx to host |
537.72 kbps 67.22 kBytes/s |
188.75 kbps 23.59 kBytes/s |
441.48 kbps 55.19 kBytes/s |
525.27 kbps 65.66 kBytes/s |
Rx from host |
575.82 kbps 71.98 kBytes/s |
189.66 kbps 23.71 kBytes/s |
417.83 kbps 52.23 kBytes/s |
381.8 kbps 47.73 kBytes/s |
Device |
Host |
|||
|---|---|---|---|---|
DA14531-01 |
DA14531 |
iPhone XR |
Samsung A52S |
One Plus 7Pro |
Tx to host |
537.855 kbps 67.23 kB/s |
188.49 kbps 23.56 kB/s |
433.45 kbps 54.18 kB/s |
494.28 kbps 61.79 kB/s |
Rx from host |
576.06 kbps 72.01 kB/s |
185.05 kbps 23.13 kB/s |
410.87 kbps 51.36 kB/s |
380.35 kbps 47.54 kB/s |
Device |
Host |
|||
|---|---|---|---|---|
DA14535 |
DA14535 |
iPhone XR |
Samsung A52S |
One Plus 7Pro |
Tx to host |
537.085 kbps 67.14 kBytes/s |
189.04 kbps 23.63 kBytes/s |
432.85 kbps 54.11 kBytes/s |
534.67 kbps 66.83 kBytes/s |
Rx from host |
575.94 kbps 71.99 kBytes/s |
186.36 kbps 23.3 kBytes/s |
413.74 kbps 51.72 kBytes/s |
383.2 kbps 47.9 kBytes/s |
Device |
Host |
|||
|---|---|---|---|---|
DA14585 |
DA14581 |
iPhone XR |
Samsung A52S |
One Plus 7Pro |
Tx to host |
537.085 kbps 67.14 kBytes/s |
193.6 kbps 24.2 kBytes/s |
450.66 kbps 56.33 kBytes/s |
537.68 kbps 67.21 kBytes/s |
Rx from host |
588.22 kbps 73.53 kBytes/s |
186.35 kbps 23.29 kBytes/s |
410.34 kbps 51.29 kBytes/s |
374.13 kbps 46.77 kBytes/s |