11.5. List of CodesΒΆ
Code 1 - Code defining the POWER_PROFILER_TRANSFER_SIZE property
Code 2 - Code defining the USE_PV_C_BOARD property
Code 3 - CLI bundle example. Burn a bootable image on DA14531 SPI
Code 4 - CLI partition index example.
Code 5 - Change JTAG communication timeout
Code 6 - Battery Lifetime Estimator CLI sample input for DA14580/581/583 family
Code 7 - Battery Lifetime Estimator CLI sample input for DA14585/6 family
Code 8 - Battery Lifetime Estimator CLI sample input for DA1453x family
Code 9 - DA14580/581/583 family defaults
Code 10 - DA14585/6 family defaults