9.6. Support Packs¶
Support Pack is a way of resource grouping and a packaging mechanism, that SmartSnippets™ Toolbox implements. Furthermore, the group of resources and configuration files that SmartSnippets™ Toolbox requires per supported device family will be referred from now on as “Support Pack” or “SP”.
Support Packs traditionally are bundled with the Application Installers. Nevertheless, while toolbox evolves along the time, a support pack can be found available for reference in one or more of the following locations:
- As part of Application’s Installer - Bundled SP
- In a Studio injected or user provided SDK workspace - SDK SP
- Over a remote Support Package update, fetched from the Internet - Remote SP
SmartSnippets™ Toolbox can be connected to an SDK and use its resources under the following scenarios:
- When launched from SmartSnippets™ Studio, it is considered connected to the same SDK that Studio is launched with.
- When launched as standalone application and user provides a custom SP via the ‘Custom Support Pack’ button.
9.6.1. Support Pack Selection¶
When SmartSnippets™ Toolbox is launched, it selects by default all Bundled SPs, while shortly after, SP selection logic takes control. During that phase Toolbox will try to list and evaluate all available sources and decide based on given prevailing logic, which of the available support packs are going to be used.
As previously mentioned, SmartSnippets™ Toolbox can get linked with Support Packs from multiple locations.
In case that there is an SDK connection, list of devices and resources found in this specific SDK are going to be used.
Note
In case that configuration xml file of the selected SDK is not valid (e.g. resources missing), the respective remote/bundled SPs (matching the selected SDK family), are going to be used. As a common rule, the most recent SP for the SDK’s family among remote SPs and bundled SPs will be used.
If launched from SmartSnippets™ Studio and remote SPs exist (for any of the SDK families), then the remote SPs are going to be used instead of the SDK provided SPs.
In different case (no SDK association), selection process will proceed with what is available with Bundled Support Packs.
Bundled Support Packs can get always updated with Remote Support Packs in almost an automated way. Toolbox will always check for available updates and every time that there is a newer remote support pack available, it will always prompt for permission to download and use it, instead of the ones found already shipped with Toolbox’s installer (or previously updated resources).
After that, application will search for any remote SPs already downloaded from a previous session and if so, it will try to validate & patch bundled SPs with anything reported as more recent from the remote ones.
In case that SDK from SmartSnippets™ Studio is going to be used and there are more recent remote SPs available, remote SPs are going to be used instead of SDK provided ones. Information about the release dates of the SDK’s SPs can be found written to info.xml file under the SDK’s config folder. If info.xml does not exist then remote SPs are always considered as more recent.
Note
If a custom SDK/SP has been selected and the respective remote SP is newer, no remote SP will be used in this case. One exception in the above rule is the case that resources are missing from the provided Custom SP, and in such a case Toolbox will try to satisfy them by using the most recent resources found available.
Support Pack selection logic can be reviewed over the following diagram.
Figure 167 Support Pack Selection Logic
9.6.2. Support Pack Validation¶
Support Pack Validation of any type (including any user-provided custom SDK/SP), goes through the following steps:
- Validate SDK/SP configuration xml file: Verifies that the file has a valid xml format and contains certain nodes, used to indicate the family, the supported devices, the resources to be used and configuration information.
- Validate SDK/SP resources: Checks against the respective bundled resources and verifies that there are existing references to all the resources required for this family pack.
- Validate existence of SDK/SP referenced resources: Verifies that the paths to the required resources are valid and that these resources exist.
If validation fails in step 1, then there are two additional scenarios we need to examine:
- If the configuration xml file is corrupted and/or SP family cannot be extracted from it.
- If the SP family is recognized, but important entries are missing from the xml file (e.g. list of devices, entries in <toolbox_config> node, <toolbox_resources> node).
In first case, application ignores the provided SDK/SP and uses all the bundled SPs per family, while validation procedure terminates with failover operation. In second case it identifies the family (or families in case of multifamily SDK), but due to other unrecoverable errors, the selected SP cannot be used. In such a case the bundled SP/s for this family/s is going to be used instead.
Note
Validation never fully fails (except of the step 1, that selected SDK/SP can get completely dropped). If validation succeeds in step 1 but fails on any of the following steps 2 and 3, then for any of the missing resources, the respective bundled resources will be used in order for the application to proceed.
After validation gets completed with success, examined SDK/SP gets selected as the currently active SP.
Note
If libprogrammer gets replaced with a bundled resource, then uartboot.bin is going to be replaced too, or vise versa.
9.6.3. Custom Support Packs¶
User can provide to SmartSnippets™ Toolbox a custom SDK/SP using ‘Set Custom SP’ menu option under the Board Menu.
Figure 168 Support Pack Chooser
The following folder structure is expected for an SDK SP or custom SP:
Figure 169 Support Pack Structure
SmartSnippets™ Toolbox looks for the Support Pack configuration xml file inside a folder named “config”. In order to select an SDK, the user should select the root path of the SDK using the Browse button, where the config folder is located. If a custom SP has been provided as an archive or the user has created a custom SP, the same structure is expected: the user should select the custom Support Pack root folder, using the Browse button, which contains a config folder where the configuration xml file can be located. If the message “SDK configuration xml file could not be found” is presented, please make sure that the SDK/SP has the folder structure described here and that the SDK/SP root folder has been selected.
Support Pack Chooser dialog provides the following options to the user:
Browse: User can select a custom SP.
Clear selection: Clears selection and sets as selected SPs the most recent SPs per family.
OK: If pressed, then changes will take effect.
Cancel: If pressed, then changes will be ignored.
Support Pack Locations: User can view the paths of the currently selected SP per family. If visualization demonstrates unsaved changes, a dedicated message will properly inform user for this incident.
Figure 170 Support Pack Location Info
SDK/SP Validation takes place as described in previous topic, while if validation of the selected SDK/SP fails, a dedicated message description will appear at the bottom of the window, to further explain the issue.
The following image represents a case were the validation of the selected SDK just failed:
Figure 171 SDK validation failure
Note
For user provided inputs or changes, to be considered as applied, OK button needs to be pressed first.
9.6.4. Remote Support Pack Update¶
SmartSnippets™ Toolbox is enabled with a SP auto-updating mechanism to keep its resources up to date. Upon startup it will try to check if there are any newer Support Packages available on Remote Site. Once a device is selected (either manually by the user or after device detection or after loading a previous project which has a saved device) it will finally check if there are new SPs that are currently not installed (for the selected device). If need be it will eventually prompt for User permission to download/update SP resources accordingly. User can check at any time for SP updates using the Check Online for Updates menu option under the Board menu. So even if the SP update is initially ignored, the user can install it at any moment in the future.
Figure 172 Support Pack Updater
Update: Updates SP for selected family.
Ignore: Ignores update for this time only. If user ticks the ‘Do not show again’ checkbox, toolbox will never ask to update on this specific SP release.
If user choose to update on found SP, then the remote SP will get downloaded, extracted, and validated. If validation succeeds, then application will update existing SP Resources (for the selected Family) with resources from the newly fetched SP update accordingly.
For the Updating process to get completed, several minutes might be needed. If user choose to ignore such an update, then the next time that toolbox gets started and same device/family is selected, same popup will appear to request permission for updating over the same or newer SP found available.
Session can continue without any further inconvenience once this updating dialog gets completed.
Note
If user decides to use a custom SDK/SP with Toolbox, then no SP Updates will be proposed on device selection and Check Online for Updates will inform the user that SP updates are not possible while a custom SDK is being used.
Figure 173 SP Updates not available with custom SPs