DA1453x / DA1458x Tutorial Create a Custom GATT Profile

Hint

This tutorial will cover SDK6 family products (DA1453x and DA1458x)

  • DA1453x is referring to DA14531-00, DA14531-01, DA14530 and DA14535.

  • The DA14531-00 is the main DA14531 device. The -00 is just a new naming to introduce the variant DA14531-01. The DA14531-01 is a ROM variant of the main DA14531-00.

  • The DA14535 is a DA14531 upgrade.

  • DA1458x is referring to DA14585 and DA14586.

Contents