Manufacturing considerations
Crystal trimming
For the DA1469x based devices with WiRa functionality enabled is it critically important to have the crystal 32MHz trimmed within 2 ppm.
Antenna
Radiation pattern
Antenna radiation pattern has a significant impact on the WiRa performance. It is important to select an antenna with a radiation pattern as omnidirectional as possible. It is also recommended for the antenna to have a flat group delay across the BLE frequency band (linear phase response), with the group delay showing as small dependence as possible on angle.
It is possible to implement a suitable antenna as a chip ceramic and PCB trace antenna.
Distance offset trimming
The board design will dictate the delay from the antenna to the demodulator. This infers a static offset in the distance measurement. The software can compensate for this and there’s a parameter stored in the configuration partition of the flash to set it correctly. The board needs to be characterized in order to allow the correct offset to be programmed in production.
Battery
The battery profile needs to be setup correctly in the custom_charging_profile.h file to allow the charge current to be correct for your chosen battery.
Device parameters
Please refer to the Device parameters in order to setup correctly the non-volatile parameters during production.