1. Introduction
1.1. Before You Start
- Before you start you need to:
Install the Keil µVision IDE 5.
Download the latest SDK version for DA1453x and DA14585/DA14586.
Additionally, for this tutorial, either a DA14531 DevkitP or USB Development kit , DA1453x DevkitP or a DA14585 Devkitp is required.
- The goal of this tutorial is not to cover every detail related to debugging but to:
Show how to use serial port for debugging.
Provide a few possible ways of analysing hard-fault.
Hint
This document is applicable to SDK6 (DA14585/6 and DA1453x) if it is not mentioned specifically for a particular application.
DA1453x is referring to DA14531-00, DA14531-01, DA14530 and DA14535.
DA1458x is referring to DA14585 and DA14586.