Logo
  • 1. Introduction
  • 2. Clone FreeRTOS retarget Project
  • 3. Implementation
  • 4. Handling Multiple Interruption Sources
External Interrupt
  • »
  • External Interruption Tutorial

External Interruption Tutorial

Contents

  • 1. Introduction
    • 1.1. Before You Start
    • 1.2. External Interrupt
    • 1.3. Working Demonstration
  • 2. Clone FreeRTOS retarget Project
  • 3. Implementation
    • 3.1. Existing Application
    • 3.2. Configure the GPIO Generating Interrupt
    • 3.3. Set up the Wake-Up Timer
    • 3.4. Handle the Interrupt
    • 3.5. Using the Notification
    • 3.6. Testing
  • 4. Handling Multiple Interruption Sources
    • 4.1. Latching the Interrupt Source
    • 4.2. Configuring Additional Sources
    • 4.3. Handling the Interrupt
Next

© Copyright 2022, Renesas Electronics Corporation.