........................................................................................................................ .. .. INITIAL FLASH .. ........................................................................................................................ . . Using device with id 480063671 . Using SDK from C:\Users\blauret\dev\SDK680\secure_boot\DA1468x_DA15xxx_SDK_1.0.12.1078 . cli_programmer from "C:\Users\blauret\dev\SDK680\secure_boot\DA1468x_DA15xxx_SDK_1.0.12.1078\binaries\cli_programmer.exe" . image file C:\Users\blauret\dev\SDK680\secure_boot\DA1468x_DA15xxx_SDK_1.0.12.1078\projects\dk_apps\demos\pxp_reporter/DA14683-00-Release_QSPI_SUOTA/pxp_reporter.bin . boot loader C:\Users\blauret\dev\SDK680\secure_boot\DA1468x_DA15xxx_SDK_1.0.12.1078\sdk/bsp/system/loaders/ble_suota_loader\DA14683-00-Release_OTP_Secure\ble_suota_loader.bin ........................................................................................................................ .. .. Preparing image file application_image.img .. ........................................................................................................................ . Using SDK from C:\Users\blauret\dev\SDK680\secure_boot\DA1468x_DA15xxx_SDK_1.0.12.1078 ........................................................................................................................ .. .. Erasing bootloader area .. ........................................................................................................................ cli_programmer 1.25 Copyright (c) 2015-2017 Dialog Semiconductor bootloader file not specified, using internal uartboot.bin done. ........................................................................................................................ .. .. Erasing partition table .. ........................................................................................................................ cli_programmer 1.25 Copyright (c) 2015-2017 Dialog Semiconductor bootloader file not specified, using internal uartboot.bin done. ........................................................................................................................ .. .. Writing application image C:\Users\blauret\dev\SDK680\secure_boot\DA1468x_DA15xxx_SDK_1.0.12.1078\projects\dk_apps\demos\pxp_reporter/DA14683-00-Release_QSPI_SUOTA/pxp_reporter.bin .. ........................................................................................................................ cli_programmer 1.25 Copyright (c) 2015-2017 Dialog Semiconductor bootloader file not specified, using internal uartboot.bin Writing to address: 0x00020000 offset: 0x00000000 chunk size: 0x00002000 Writing to address: 0x00020000 offset: 0x00002000 chunk size: 0x00002000 Writing to address: 0x00020000 offset: 0x00004000 chunk size: 0x00002000 Writing to address: 0x00020000 offset: 0x00006000 chunk size: 0x00002000 Writing to address: 0x00020000 offset: 0x00008000 chunk size: 0x00002000 Writing to address: 0x00020000 offset: 0x0000a000 chunk size: 0x00002000 Writing to address: 0x00020000 offset: 0x0000c000 chunk size: 0x00002000 Writing to address: 0x00020000 offset: 0x0000e000 chunk size: 0x00002000 Writing to address: 0x00020000 offset: 0x00010000 chunk size: 0x00002000 Writing to address: 0x00020000 offset: 0x00012000 chunk size: 0x00002000 Writing to address: 0x00020000 offset: 0x00014000 chunk size: 0x00001c70 done. ........................................................................................................................ .. .. Writing image header application_image.img .. ........................................................................................................................ cli_programmer 1.25 Copyright (c) 2015-2017 Dialog Semiconductor bootloader file not specified, using internal uartboot.bin Writing to address: 0x0001f000 offset: 0x00000000 chunk size: 0x00000400 done. ........................................................................................................................ .. .. Writing bootloader .. ........................................................................................................................ cli_programmer 1.25 Copyright (c) 2015-2017 Dialog Semiconductor bootloader file not specified, using internal uartboot.bin Reading from address: 0x50003200 offset: 0x00000000 chunk size: 0x00000001 Reading from address: 0x50003201 offset: 0x00000000 chunk size: 0x00000001 Reading from address: 0x50003202 offset: 0x00000000 chunk size: 0x00000001 Reading from address: 0x50003204 offset: 0x00000000 chunk size: 0x00000001 Reading from address: 0x5000320a offset: 0x00000000 chunk size: 0x00000001 done. ........................................................................................................................ .. .. Writing symmetric keys .. ........................................................................................................................ cli_programmer 1.25 Copyright (c) 2015-2017 Dialog Semiconductor bootloader file not specified, using internal uartboot.bin Symmetric key #0 and its bit inversion written properly. done. cli_programmer 1.25 Copyright (c) 2015-2017 Dialog Semiconductor bootloader file not specified, using internal uartboot.bin Symmetric key #1 and its bit inversion written properly. done. cli_programmer 1.25 Copyright (c) 2015-2017 Dialog Semiconductor bootloader file not specified, using internal uartboot.bin Symmetric key #2 and its bit inversion written properly. done. cli_programmer 1.25 Copyright (c) 2015-2017 Dialog Semiconductor bootloader file not specified, using internal uartboot.bin Symmetric key #3 and its bit inversion written properly. done. cli_programmer 1.25 Copyright (c) 2015-2017 Dialog Semiconductor bootloader file not specified, using internal uartboot.bin Symmetric key #4 and its bit inversion written properly. done. cli_programmer 1.25 Copyright (c) 2015-2017 Dialog Semiconductor bootloader file not specified, using internal uartboot.bin Symmetric key #5 and its bit inversion written properly. done. cli_programmer 1.25 Copyright (c) 2015-2017 Dialog Semiconductor bootloader file not specified, using internal uartboot.bin Symmetric key #6 and its bit inversion written properly. done. cli_programmer 1.25 Copyright (c) 2015-2017 Dialog Semiconductor bootloader file not specified, using internal uartboot.bin Symmetric key #7 and its bit inversion written properly. done. ........................................................................................................................ .. .. Writing asymmetric keys .. ........................................................................................................................ cli_programmer 1.25 Copyright (c) 2015-2017 Dialog Semiconductor bootloader file not specified, using internal uartboot.bin Asymmetric key #0 and its bit inversion written properly. done. cli_programmer 1.25 Copyright (c) 2015-2017 Dialog Semiconductor bootloader file not specified, using internal uartboot.bin Asymmetric key #1 and its bit inversion written properly. done. cli_programmer 1.25 Copyright (c) 2015-2017 Dialog Semiconductor bootloader file not specified, using internal uartboot.bin Asymmetric key #2 and its bit inversion written properly. done. cli_programmer 1.25 Copyright (c) 2015-2017 Dialog Semiconductor bootloader file not specified, using internal uartboot.bin Asymmetric key #3 and its bit inversion written properly. done. cli_programmer 1.25 Copyright (c) 2015-2017 Dialog Semiconductor bootloader file not specified, using internal uartboot.bin done. cli_programmer 1.25 Copyright (c) 2015-2017 Dialog Semiconductor bootloader file not specified, using internal uartboot.bin done. . ........................................................................................................................ .. .. FINISHED .. ........................................................................................................................