5. DA14592 – Module-DEVKIT hardware
The SmartBond DA14592 Module is based on the Renesas DA14592 SoC. With an integrated 32 Mbit flash, 32 MHz XTAL and a printed antenna, the module enables a faster time to market at reduced development costs.
The module, as seen also in Figure 5 , is comprised of:
32 Mbit SPI FLASH
32 MHz XTAL
Decoupling capacitors
A power inductor
A CLC filter and matching components for the printed antenna
Figure 3 The DA14592 Module (Front)
Figure 4 The DA14592 Module (Back)
Figure 5 The DA14592 Module Block Diagram
6. Connecting to the Mother Board
Figure 6 shows how the DA14592 Module is connected to the DA14592 mother board.
Figure 6 The DA14592 Module-DEVKIT