1. Overview

The Renesas SmartBond™ DA14535 (core ARM Cortex® M0+) development Kit is intended to drive software and hardware development on the DA14535 family. Please refer to Renesas DA14535 product page for detailed features list. The development kit main features are:

  • Embedded Segger J-Link™ debugger

  • Onboard Flash (Adesto / AT25DF021A / 2M-Bit)

  • User switches

  • Header connectors to access the GPIOs

  • User LEDs

  • mikroBUS™ socket to allow to utilize a range of click boards™.

The SmartBond™ DA14535 USB Kit is delivered preloaded with a demonstration application enabling a Bluetooth peripheral application.

../_images/usb_kit.svg

2. Operation of Peripheral Application

2.1. Prerequisites

Minimum hardware requirements:

  • Windows Operating System, 1 GHz, 32-bit or 64-bit processor
    • 1 GB of system memory (RAM)

  • DA14535 USB Kit

  • Serial-port terminal software (for example, Tera Term)

  • To find and connect to the DA14535 device you need to Download a BLE scanner for instance LightBlue Explorer Application for iOS or Android .

2.2. How to run the Demo

../_images/usb_attached.jpg

Figure 1 DA14535 USB Kit connected to the PC

  • Observe the print out: The application is reading the unique random address from OTP and generate the BD address and sent it to the UART every 2 second.

The Figure 2 is showing the expected results:

Note

  • The LED is Blinking to indicate that the demo is running on the Board.

  • The BD address is unique per Board.

../_images/uart_print.jpg

Figure 2 BLE BD adress printed each 2 second

3. Resources

In order to start developing on the DA14531 Kit you should get the resources linked below from the DA14531 family product page:

For more information about the development environment and starting to develop your application, you can check: