3.4. Flash DataΒΆ
The tool allows programming the complete FLASH memory.
Figure 52 Flash Data tool
The user can select the FLASH memory to work with from the drop down list on the left. The start and end addresses are updated according to the selected memory start address and its size. The user can specify the address to read from or to burn to by editing the start address. The user can specify the memory region to be erased by editing the start and end addresses. Content to Burn table presents the data of the file that is going to be burned to the memory. Content Read table presents the memory contents. The tool provides the following options to the user:
- Connect: Establishes connection to the target device by initializing communication interface and downloading appropriate FW required for the communication to the target.
- Import from File: Imports data from .hex or .bin file into Content to Burn table.
- Export to File: Exports contents of Contents Read or Content to Burn table to .hex or .bin file.
- Read: Reads 32 Kb of data from memory starting from start address and presents them in Content Read table.
- Burn: Burns data of Content to Burn table at start address. Then reads memory at start address and refreshes Content Read table.
- Erase: Erases memory region between start address and end address. Then reads memory at start address and refreshes Content Read table. Note that for DA1459x family devices the user is advised to not erase the Configuration Script from memory in order not to loose important trim/calibration values. If CS is detected in the memory region to be erased, the user will be asked if he/she wants to erase the CS too (Figure 7). If no is selected, which is the default option, only the sectors after the CS end will be erased. If yes is selected, the selected memory region, including the CS, will be erased.
- Verify Erase: If checked, after erase it is verified that all the bytes of the memory segment between start and end address are empty.