1. Example description

The example can be downloaded from Here.

This example illustrates to the user, how to use SEGGER RTT in conjunction with the DA145xx family.

2. HW and SW configuration

This example runs on the BLE Smart SoC (System on Chip) devices:

  • DA14585/DA14586 or DA14531 daughter board + DA145xxDEVKT-P PRO-Motherboard.
  • DA14585/DA14586 Basic development Kit.
  • DA14531 USB Kit

The user manuals for the development kits can be found:

  • Hardware configuration DA14585 using the DA145xxDEVKT-P PRO-Motherboard

    • No special Hardware configuration is needed other than a physical link to the chip via JTAG.
  • Software configuration

    • This example requires:
    • SDK6.0.12 or Newer (Older versions of SDK6 require minimal changes)
    • SEGGER’s J-Link tools should be downloaded and installed.

3. How to run the example

3.1. Setup

Before launching the Keil project, make sure to link the SDK and project environment using the Python linker script dlg_make_keil_vx.xxx. More information here.

  1. Start Keil using the user_segger_rtt_periph Keil project file.

  2. Expand the dialog shown in the red box in the image below.

    Expand_Select_Device

  3. Select your target device: DA14531, DA14585, DA14586

  4. Compile (F7) and launch (ctrl + F5) the example.\

  5. You will need the address of the SEGGER RTT Control Block for the next step. This project automatically locates the CB in the beginning of retention RAM so the user doesn’t need to locate the address after each build. If using SDK 6.0.14, the default address is commented in segger_rtt/SEGGER_SWD_printf.h copy this address and proceed to step 8. If not using SDK 6.0.14, then proceed to step 6.

  6. Right click on the project in the Project window and select ‘Open Map File’

    Open_Map_File

  7. In the map file, use CTRL+F and search for _SEGGER_RTT and copy this address.

    Segger_CB_addr

  8. Open Segger J-Link RTT Viewer and a prompt screen will open. Be sure the following settings match - USB, Target (DA14531 - M0+, DA14585/86 - M0), and SWD. For the RTT Control Block, use the address found in steps 5-7. Once this is completed, Press OK.

    Segger_RTT_Viewer_Config

3.2. Running the Example - Scan and Connect

  1. Start a debugging session.

    keil-start-debug

  2. Make the RTT Viewer terminal window visible and you should see Data printing out every second. Additionally, you will see debug information displayed on startup, connect, and disconnect.

    RTT_Viewer_Output

4. Including RTT in another Project

  1. Copy the segger_rtt folder and place it in the same directory as your src folder.

  2. Right Click on the project in the Project Window and Select Manage Project Items.

  3. Under Groups, select New (Insert) and name it segger_rtt.

    Add_Group

  4. In the project Window, right click on segger_rtt window and select Add Existing Files to Group ‘segger_rtt’.

  5. Navigate to the RTT folder and add all files from this folder location.

  6. Add this folder to the include directories.

    • Right Click on the project and select Options for Target ‘DA145xx’.
    • Go to C/C++
    • Expand the Include Paths
    • Selecet New (Insert)
    • For this example, the include path is at ...\segger_rtt\RTT

    Include_Path

  7. In user_config Project folder, navigate to da1458x_config_advanced.h. The CFG_RET_DATA_SIZE will need updated, add the following lines of code and replace the current defintition of CFG_RET_DATA_SIZE. Be sure to include this definition in both DA14531 and DA14585/6 settings.

    // / Enables SEGGER RTT Debugging / / NOTE: Enabling increases the size of retetention DATA / // #define CFG_SWD_PRINTF // / Maximum retention memory in bytes. The base address of the retention data is calculated from the selected / / size. / //

    #ifdef CFG_SWD_PRINTF #define CFG_RET_DATA_SIZE (2048 + 0x4b8) #else #define CFG_RET_DATA_SIZE (2048) #endif

5. Known Limitations

6. License


Copyright (c) 2021 Dialog Semiconductor. All rights reserved.

This software (“Software”) is owned by Dialog Semiconductor. By using this Software you agree that Dialog Semiconductor retains all intellectual property and proprietary rights in and to this Software and any use, reproduction, disclosure or distribution of the Software without express written permission or a license agreement from Dialog Semiconductor is strictly prohibited. This Software is solely for use on or in conjunction with Dialog Semiconductor products.

EXCEPT AS OTHERWISE PROVIDED IN A LICENSE AGREEMENT BETWEEN THE PARTIES OR AS REQUIRED BY LAW, THE SOFTWARE IS PROVIDED “AS IS”, WITHOUT WARRANTY OF ANY KIND, EXPRESS OR IMPLIED, INCLUDING BUT NOT LIMITED TO THE WARRANTIES OF MERCHANTABILITY, FITNESS FOR A PARTICULAR PURPOSE AND NON-INFRINGEMENT. EXCEPT AS OTHERWISE PROVIDED IN A LICENSE AGREEMENT BETWEEN THE PARTIES OR BY LAW, IN NO EVENT SHALL DIALOG SEMICONDUCTOR BE LIABLE FOR ANY DIRECT, SPECIAL, INDIRECT, INCIDENTAL, OR CONSEQUENTIAL DAMAGES, OR ANY DAMAGES WHATSOEVER RESULTING FROM LOSS OF USE, DATA OR PROFITS, WHETHER IN AN ACTION OF CONTRACT, NEGLIGENCE OR OTHER TORTIOUS ACTION, ARISING OUT OF OR IN CONNECTION WITH THE USE OR PERFORMANCE OF THE SOFTWARE.