1. Example description¶
The example demonstrates an optimized software implementation for ibeacon on the DA14531, it can be downloaded from A14531 Power optimized Dynamic advertising
The example is an update of the ibeacon SW, below the main modifications, basically we demonstrate how to:
- Alternate Static random address: change the device address in every advertising event
- Alternate Tx output power level: change the Tx output power level in every advertising event
- Alternate User advertising data: change the Beacon advertising payload in every advertising event
A new ibeacon structure has been created to allow the alternating and the advertising interval is set to 10 s.
Because the example needs changes into the SDK we are providing within the source directory for all the modified files: src\modified_files
/* Set the advertising rate */
#define ADV_INTERVAL_ms 10000
ibeacon_adv_payload_t adv_payload;
ibeacon_adv_payload_t_new adv_payload_new;
if(change_bd_addr_flag % 2)
{
user_app_adv_start();
/* Alternate User advertising data*/
memcpy(store_adv_data, &adv_payload, sizeof(ibeacon_adv_payload_t));
store_adv_data_len = sizeof(ibeacon_adv_payload_t);
/* Alternate Tx output power, Set output power to maximum value (0dBm) */
rf_pa_pwr_set(RF_TX_PWR_LVL_0d0);
/* Alternate Static random address */
llm_le_env.rand_add.addr[0] = 0x11;
llm_le_env.rand_add.addr[1] = 0x12;
llm_le_env.rand_add.addr[2] = 0x13;
llm_le_env.rand_add.addr[3] = 0x14;
llm_le_env.rand_add.addr[4] = 0x15;
llm_le_env.rand_add.addr[5] = 0x16;
}
else
{
user_app_adv_start_new();
/* Alternate User advertising data*/
memcpy(store_adv_data, &adv_payload_new, sizeof(ibeacon_adv_payload_t_new));
store_adv_data_len = sizeof(ibeacon_adv_payload_t_new);
/* Alternate Tx output power, Set output power to maximum value (+2.5dBm) */
rf_pa_pwr_set(RF_TX_PWR_LVL_PLUS_2d5);
/* Alternate Static random address */
llm_le_env.rand_add.addr[0] = 0x01;
llm_le_env.rand_add.addr[1] = 0x02;
llm_le_env.rand_add.addr[2] = 0x03;
llm_le_env.rand_add.addr[3] = 0x04;
llm_le_env.rand_add.addr[4] = 0x05;
llm_le_env.rand_add.addr[5] = 0x06;
}

In this example we are showing also how to tune the DA14531 for a minimum current consumption. When the changes are applied to the SDK, the current consumption will be decreased by 18%.
Below the list of changes for power improvement:
- Optimize the time between Tx pulses
rwble.c :
__BLEIRQ void rwble_isr(void)
{
.....
/* Optimize the time between Tx pulses */
ble_advtim_set (500);
}

- Lower the clock speed on the AMBA when sleep preparation
arch_system.c :
__WEAK bool app_use_lower_clocks_check(void)
{
return true;
}

- Remove RCX read and calibration
arch_main.c :
#if defined (__DA14531__)
// rcx20_read_freq(false);
#endif
- Reduce RF calibration routine
arch_system.c :
void conditionally_run_radio_cals(void)
{
#if defined (__DA14531__)
// 531 case
uint32_t current_time = lld_evt_time_get();
if (current_time < last_temp_time)
{
last_temp_time = 0;
}
if ((current_time - last_temp_time) >= 500000)
{
- Reduce XTAL32M wait time
otp_cs.c :
#define XTAL32M_WAIT_TRIM_TIME_USEC (500) // 500 usec
- Optimize xtal start-up time
arch.h :
#if defined (__DA14531__)
#define HW_STARTUP_TIME_IN_XTAL32K_CYCLES (11) // 11 LP clocks for startup state machine handling
#define HW_STARTUP_TIME_IN_RCX_CYCLES (7) // 7 LP clocks for startup state machine handling
#define RCX_BLE_PWR_UP_TO_SLP_IRQ_USEC (60)
#define XTAL32K_BLE_PWR_UP_TO_SLP_IRQ_USEC (45)
#endif
The results are given in the below screenshots:
- Average power consumption with no software optimization : 2,77 uA

- Average power consumption with software optimization : 2,27 uA

- Average power consumption during sleep : 1,2 uA

Estimate battery life
Battery life can be calculated when you know the average current consumption of the device and the energy capacity of your battery. Battery Lifetime Estimator tool can be used and it can be loaded (from the Smartsnippets toolbox) by selecting the “Power Monitor” under Layout in the Toolbar or the “Battery Lifetime Estimator” under Tools.
2. HW and SW configuration¶
- Hardware configuration
- Software configuration
- This example requires:
- Smartsnippets Studio 2.0.14 (or later)
- SDK6.0.14 (or later)
- SEGGER’s J-Link tools should be downloaded and installed.
- This example requires:
3. How to run the example¶
For initial setup of the example please refer to this section of the dialog support portal.
3.1. Initial Setup¶
- Build and download the example using the Keil IDE.
- Run the example using the Keil debugger.
- Use a Smart Device running an App such as Locate to view the beacons transmitted by the DA14531.
4. Known Limitations¶
- There are no known limitations for this example. But you can check and refer to the following application note for known hardware limitations for DA14531 devices: DA14531 hardware limitations
- Dialog Software Forum Link.
- You can also refer to the troubleshooting section in the Getting Started with the DA14531 PRO Development Kit.
5. License¶
Copyright (c) 2020 Dialog Semiconductor. All rights reserved.
This software (“Software”) is owned by Dialog Semiconductor. By using this Software you agree that Dialog Semiconductor retains all intellectual property and proprietary rights in and to this Software and any use, reproduction, disclosure or distribution of the Software without express written permission or a license agreement from Dialog Semiconductor is strictly prohibited. This Software is solely for use on or in conjunction with Dialog Semiconductor products.
EXCEPT AS OTHERWISE PROVIDED IN A LICENSE AGREEMENT BETWEEN THE PARTIES OR AS REQUIRED BY LAW, THE SOFTWARE IS PROVIDED “AS IS”, WITHOUT WARRANTY OF ANY KIND, EXPRESS OR IMPLIED, INCLUDING BUT NOT LIMITED TO THE WARRANTIES OF MERCHANTABILITY, FITNESS FOR A PARTICULAR PURPOSE AND NON-INFRINGEMENT. EXCEPT AS OTHERWISE PROVIDED IN A LICENSE AGREEMENT BETWEEN THE PARTIES OR BY LAW, IN NO EVENT SHALL DIALOG SEMICONDUCTOR BE LIABLE FOR ANY DIRECT, SPECIAL, INDIRECT, INCIDENTAL, OR CONSEQUENTIAL DAMAGES, OR ANY DAMAGES WHATSOEVER RESULTING FROM LOSS OF USE, DATA OR PROFITS, WHETHER IN AN ACTION OF CONTRACT, NEGLIGENCE OR OTHER TORTIOUS ACTION, ARISING OUT OF OR IN CONNECTION WITH THE USE OR PERFORMANCE OF THE SOFTWARE.