1. Example description

Simple example showing how to implement an iBeacon on the DA14531, DA14585/586. All beacon payload parameters (advertising interval, UUID etc.) are easily configurable from within the user application (user_app.c).

The example is configured to use a random static Bluetooth Device address (BD address). This is generated upon power on or reset and will remain static throughout the life of the device. It is also guaranteed to be unique on each DA14531 or DA14585/586 device (i.e. a different BD address will be generated on each DA14531 or DA14585/586 on which this is example is run).

By default the output power is set to 0dBm. This can be increased to +2.5dBm (only for the DA14531) by defining the macro TX_POWER_2d5Bm (see the macro definitions at the start of the user_app.c file).

Note The example can be downloaded from Here.

2. HW and SW configuration

  • Hardware configuration

  • This example runs on the DA14531 or DA14585/DA14586 Bluetooth Smart SoC device.

  • For running the example on DA14531, a USB Kit or PRO Development kit along with a DA14531 Daughter Board is needed.

  • For running the example on DA14585/586, a PRO Development kit along with a DA14585 or a DA14586 Daughter Board is needed.

  • Software configuration

This example requires:

  • Smartsnippets Studio 2.0.10 (or later)

  • SDK6.0.14 (or later)

  • SEGGER’s J-Link tools should be downloaded and installed.

3. How to run the example

For initial setup of the example please refer to this section of the dialog support portal.

3.1. Initial Setup

  1. Build and download the example using the Keil IDE.

  2. Run the example using the Keil debugger.

  3. Use a Smart Device running an App such as Locate to view the beacons transmitted by the device.

4. Known Limitations

5. License


Copyright (c) 2021 Dialog Semiconductor. All rights reserved.

This software (“Software”) is owned by Dialog Semiconductor. By using this Software you agree that Dialog Semiconductor retains all intellectual property and proprietary rights in and to this Software and any use, reproduction, disclosure or distribution of the Software without express written permission or a license agreement from Dialog Semiconductor is strictly prohibited. This Software is solely for use on or in conjunction with Dialog Semiconductor products.

EXCEPT AS OTHERWISE PROVIDED IN A LICENSE AGREEMENT BETWEEN THE PARTIES OR AS REQUIRED BY LAW, THE SOFTWARE IS PROVIDED “AS IS”, WITHOUT WARRANTY OF ANY KIND, EXPRESS OR IMPLIED, INCLUDING BUT NOT LIMITED TO THE WARRANTIES OF MERCHANTABILITY, FITNESS FOR A PARTICULAR PURPOSE AND NON-INFRINGEMENT. EXCEPT AS OTHERWISE PROVIDED IN A LICENSE AGREEMENT BETWEEN THE PARTIES OR BY LAW, IN NO EVENT SHALL DIALOG SEMICONDUCTOR BE LIABLE FOR ANY DIRECT, SPECIAL, INDIRECT, INCIDENTAL, OR CONSEQUENTIAL DAMAGES, OR ANY DAMAGES WHATSOEVER RESULTING FROM LOSS OF USE, DATA OR PROFITS, WHETHER IN AN ACTION OF CONTRACT, NEGLIGENCE OR OTHER TORTIOUS ACTION, ARISING OUT OF OR IN CONNECTION WITH THE USE OR PERFORMANCE OF THE SOFTWARE.