1. Example description¶
This is a simple implementation of a basic blinky application that runs “bare metal” without FreeRTOS. Bluetooth LE is NOT supported by this example.
Note The example can be downloaded from Here.
2. HW and SW configuration¶
Hardware configuration
This example runs on DA1469x Bluetooth Smart SoC devices.
A PRO or USB Development kit is needed for this example.
Connect the Development kit to the host computer.
Software configuration
This example requires:
Smartsnippets Studio 2.0.16 or greater
SDK 10.0.10.118 or greater
SEGGER J-Link tools should be downloaded and installed.
3. How to run the example¶
3.1. Initial Setup¶
Compile and launch RAM or QSPI target
Run from RAM or load in the flash
The RGB LED is blinking RED on/off every second.
4. Known Limitations¶
There are no known limitations for this example.
Dialog Software Forum link.
5. License¶
Copyright (c) 2021 Dialog Semiconductor. All rights reserved.
This software (“Software”) is owned by Dialog Semiconductor. By using this Software you agree that Dialog Semiconductor retains all intellectual property and proprietary rights in and to this Software and any use, reproduction, disclosure or distribution of the Software without express written permission or a license agreement from Dialog Semiconductor is strictly prohibited. This Software is solely for use on or in conjunction with Dialog Semiconductor products.
EXCEPT AS OTHERWISE PROVIDED IN A LICENSE AGREEMENT BETWEEN THE PARTIES OR AS REQUIRED BY LAW, THE SOFTWARE IS PROVIDED “AS IS”, WITHOUT WARRANTY OF ANY KIND, EXPRESS OR IMPLIED, INCLUDING BUT NOT LIMITED TO THE WARRANTIES OF MERCHANTABILITY, FITNESS FOR A PARTICULAR PURPOSE AND NON-INFRINGEMENT. EXCEPT AS OTHERWISE PROVIDED IN A LICENSE AGREEMENT BETWEEN THE PARTIES OR BY LAW, IN NO EVENT SHALL DIALOG SEMICONDUCTOR BE LIABLE FOR ANY DIRECT, SPECIAL, INDIRECT, INCIDENTAL, OR CONSEQUENTIAL DAMAGES, OR ANY DAMAGES WHATSOEVER RESULTING FROM LOSS OF USE, DATA OR PROFITS, WHETHER IN AN ACTION OF CONTRACT, NEGLIGENCE OR OTHER TORTIOUS ACTION, ARISING OUT OF OR IN CONNECTION WITH THE USE OR PERFORMANCE OF THE SOFTWARE.