1. Example description¶
This sample code aims at demonstrating the crypto engine. The DA1469x family of devices incorporates a crypto engine capable of performing AES as well as HASH operations. Please note that the aforementioned functionalities work complementary, that is, either AES or HASH mode can be enabled at a time. A dedicated DMA engine is used for transferring data to/from TxFIFO and RxFIFO respectively. One interesting feature of the crypto engine is its ability to process fragmented data, that is, data residing at different memory locations. The sample code provides APIs that hide the complexity of utilizing the crypto engine. By default, two tasks are being created: one task responsible for demonstrating AES operations and one task responsible for HASH operations. Both of them can be enabled/disabled using the AES_CRYPTO_ENABLE and HASH_CRYPTO_ENABLE macros respectively.
Note The example can be downloaded from Here.
1.1. HW & SW Configurations¶
Hardware Configurations
This example runs on a DA1469x Bluetooth Smart SoC.
A DA1469x Pro Development Kit is needed for this example.
Software Configurations
Download the latest SDK version for the DA1469x family of devices (10.0.10)
SEGGER’s J-Link tools should be downloaded and installed.
2. How to run the example¶
2.1. Initial Setup¶
Download the source code from the Support Website
Import the project into your workspace.
Connect the target device to your host PC.
Compile the code (either in Release or Debug mode) and load it into the chip.
Open a serial terminal (115200/8 - N - 1)
Press the reset button on DA1469x daughterboard to start executing the application.
If SERIAL_CONSOLE_ENABLE macro is set to one (by default enabled) you should expect to get the following output on the serial console:


3. Known Limitations¶
There are no known limitations for this sample code.
4. License¶
Copyright (c) 2021 Dialog Semiconductor. All rights reserved.
This software (“Software”) is owned by Dialog Semiconductor. By using this Software you agree that Dialog Semiconductor retains all intellectual property and proprietary rights in and to this Software and any use, reproduction, disclosure or distribution of the Software without express written permission or a license agreement from Dialog Semiconductor is strictly prohibited. This Software is solely for use on or in conjunction with Dialog Semiconductor products.
EXCEPT AS OTHERWISE PROVIDED IN A LICENSE AGREEMENT BETWEEN THE PARTIES OR AS REQUIRED BY LAW, THE SOFTWARE IS PROVIDED “AS IS”, WITHOUT WARRANTY OF ANY KIND, EXPRESS OR IMPLIED, INCLUDING BUT NOT LIMITED TO THE WARRANTIES OF MERCHANTABILITY, FITNESS FOR A PARTICULAR PURPOSE AND NON-INFRINGEMENT. EXCEPT AS OTHERWISE PROVIDED IN A LICENSE AGREEMENT BETWEEN THE PARTIES OR BY LAW, IN NO EVENT SHALL DIALOG SEMICONDUCTOR BE LIABLE FOR ANY DIRECT, SPECIAL, INDIRECT, INCIDENTAL, OR CONSEQUENTIAL DAMAGES, OR ANY DAMAGES WHATSOEVER RESULTING FROM LOSS OF USE, DATA OR PROFITS, WHETHER IN AN ACTION OF CONTRACT, NEGLIGENCE OR OTHER TORTIOUS ACTION, ARISING OUT OF OR IN CONNECTION WITH THE USE OR PERFORMANCE OF THE SOFTWARE.