High current Consumption in LPCD-Mode

ID: NCI100R-100

Status: Open

First reported: PTX130R AIS SDK v2.0.0

Fixed in: Future SDK Version

Description

If Poll- and Listen-mode are enabled together with LPCD-mode during the RF-Discovery procedure, it may lead to a higher current consumption on some systems.

Workaround

None - will be fixed in future SDK Version. Actual functionality (using Poll- and/or Listen-mode together with LPCD) not impacted.