Overview of D/AVE 2D driver V3.18
| Driver Overview | Overview of D/AVE 2D driver V3.18 |
| Coding conventions | Quickinfo about Dave2d Driver implementation |
| Concept | Basic objects and principles |
| Sample code | Simple example of using the dave driver |
Quickinfo about Dave2d Driver implementation
Basic objects and principles
The driver allows direct access to all hardware features. Functionality not directly supported by hardware is not offered (emulated) by the driver.
Simple example of using the dave driver
Further information and examples can be found in the Driver Tutorial (software/tutorial/driver_tutorial.doc).
To create a device, allocate and initialize the hardware (errorchecks omitted for clarity) :
#include "dave_driver.h"
int main()
{
void *framebuffer;
// Use the default memory management functions and register a wrapper for the normal malloc, free and msize commands of the system.
// Note: On some platforms a different memory manager for video and heap management may be required.
// A different memory manager can be chosen by calling d0_initheapmanager(..) instead of d0_initdefaultheapmanager().
d0_initdefaultheapmanager(); // initialize D/AVE driver memory management interface
d2_device *handle = d2_opendevice( 0 ); // create a device
d2_setdlistblocksize( handle, 25 ); // set blocksize for default displaylist
d2_lowlocalmemmode( handle, 20, 10 ); // systems with low local CPU memory need this mode
d2_inithw( handle, 0 ); // bind the hardwarenow we setup a 32bit 640x480 pixel framebuffer using the lowlevel driver
framebuffer = d1_allocvidmem(d2_level1interface(handle), d1_mem_display, 640*480*4); // define address and memory organisation of framebuffer d2_framebuffer( handle, framebuffer, 640, 640, 480, d2_mode_argb8888 );
using the default context we can directly start and setup our material attributes
d2_setcolor( handle, 0, 0xffffff ); // just simple white d2_setblendmode( handle, d2_bm_alpha, d2_bm_one_minus_alpha ); d2_setalphamode( handle, d2_am_constant ); d2_setalpha( handle, 0x7f ); // 50% transparency d2_setblur( handle, 4*16 );
the rendering happens inside an endless loop, as it is the case for most realtime animated graphics. In order to avoid having to deal with renderbuffers manual, we use the utility functions startframe and endframe to get automatic buffer management.
d2_point x = 320*16;
d2_point y = 240*16;
//
while (1)
{
d2_startframe( handle );
d2_clear( handle, 0x000000 ); // clear the background
d2_rendercircle( handle, x, y, 64*16, 0 ); // draw our circle
d2_endframe( handle );
x += 1;
y += 8;
}