2. Setting the Bluetooth Device Address and Device Name
Each SmartBond™ device software example uses a default Bluetooth Device (BD) Address, if the developer has not assigned a different one. This section provides a step-by-step description of how to change the BD Address and Device Name to make it suitable for your application needs. For more details, you can refer to the Bluetooth Device Address Section in DA1453x/DA1458x Tutorial SDK6 Getting Started.
2.1. Setting the BD Address
There are two types of Bluetooth Device Addresses, which are called Public Device Address and Random Device Address.
A Public Device Address is a globally unique 48-bit identifier, which consists of two fields:
The 24 most significant bits are called the Organizational Unique Identifier, and its purpose is to identify each company. It is administered by the IEEE Registration Authority.
The 24 least significant bits are assigned by the company, and they serve the purpose of identifying each device.
A Random Device Address is a privacy feature of the BLE protocol, and it helps to prevent tracking of a device. BLE provides a resolution mechanism so that only a device which holds the connection link key can identify the device.
The public address of the device is set in the CFG_NVDS_TAG_BD_ADDRESS macro in da1458x_config_advanced.h.
Considering this address : {0x02, 0x00, 0x70, 0xCA, 0xEA, 0x80}.
Code snippet:
/******************************************************************************************/
/* NVDS configuration */
/* - CFG_NVDS_TAG_BD_ADDRESS Default bdaddress. If bdaddress is written in OTP header */
/* this value is ignored */
/******************************************************************************************/
#define CFG_NVDS_TAG_BD_ADDRESS {0x02, 0x00, 0x70, 0xCA, 0xEA, 0x80}
To change the BD Address you only have to change this define. For instance, you can set it to:
Code snippet:
#define CFG_NVDS_TAG_BD_ADDRESS {0x01, 0x02, 0x03, 0x04, 0x05, 0x06}
A new device with {0x01, 0x02, 0x03, 0x04, 0x05, 0x06} as the BD Address will then show up in the list of discovered devices as shown in Figure 6 (screenshot from a BLE Scanner application).
Figure 6 Setting the BD Address
2.2. Setting the Advertised Device Name
Since it would be quite difficult for a user to identify a device using only its BD Address, BLE provides the Device Name property, which is a human-friendly
name used to tag a device. This is assigned with the USER_DEVICE_NAME macro, which can be customized in user_config.h.
This example demonstrates how to change the advertised Device Name based on the barebone example: projects/target_apps/ble_examples/ble_app_barebone.
Section “Build a DA1453x Application” of the UM-B-117: DA14531 Getting Started Guide with the PRO-Development Kit and UM-B-165: DA14535 Getting Started Guide with the PRO-Development Kit demonstrate a BLE advertising procedure. Refer to these for more details.
The barebone example demonstrates a simple barebone project which advertises its presence with customized data. Figure 7 shows an example where a smartphone operates as a Central and a DA1458x or DA1453x device as a Peripheral.
Code snippet:
/*
****************************************************************************************
*
* Device name.
*
* - If there is space left in the advertising or scan response data, the device name
* is copied there. The device name can be read at anytime by a connected peer, if
* the application supports it.
* - The Bluetooth device name can be up to 248 bytes.
*
****************************************************************************************
*/
/// Device name
#define USER_DEVICE_NAME "DLG-BRBN"
/// Device name length
#define USER_DEVICE_NAME_LEN (sizeof(USER_DEVICE_NAME)-1)
Figure 7 BLE Connection with Pro DK
To customize the advertised device name, change the macro definition as required:
Code snippet:
#define USER_DEVICE_NAME "DLG-TUTORIAL"
Then compile and download the barebone example again to see that your device name has changed.