7. UART Booting options

The boot ROM code initially configures the DA1453x UART controller with the following parameters:
  • Bits: 8

  • No parity

  • 1 stop bit

  • Baud rate: fixed at 115.2 Kbps for DA1453x

The protocol required to establish successful communication and to download the SW image into the RAM is shown in the next tables depending on the chip:

  1. The protocol starts with the DA1453x UART TX pin that transmits 0x02 (Start TX – STX).

  2. The external device is expected to answer with a 0x01 (Start of Header – SOH) byte followed by 2 more bytes (LEN_LSB, LEN_MSB), which define the length of the code to be downloaded (the first byte is the least significant, second the most significant).

  3. The DA1453x answers with 0x06 (ACK) if the 3 bytes have been received and SOH has been identified, or answers with 0x15 (NACK) if anything went wrong.

../_images/uart_boot.svg

Figure 17 Boot Protocol

After Byte number 4, the connection has been successfully established and the SW code will start to be downloaded. The next N bytes are received and put into the RAM and start at address 0x07FC0000 as shown in Table 4. Boot sequence concludes upon receiving 0x06 (ACK) via URX. checksum is calculated by XORing each byte successively, starting from an initial value of 0x00. At the end, SYS_CTRL_REG is set to remap to address zero for RAM execution (SYS_CTRL_REG``[REMAP_ADR0] = ``0x2) and to initiate a software reset (SYS_CTRL_REG``[SW_RESET] = ``0x1).

Table 4 Boot bytes

Address

Byte 3 (MSB)

Byte 2

Byte 1

Byte 0

0x07FC0000

Code byte 3

Code byte 2

Code byte 1

Code byte 0

0x07FC0004

…

…

Code byte 5

Code byte 4

7.1. Booting from 1-wire UART

The one-wire UART boot capability is introduced due to the limited amount of the GPIOs. Since the booting from UART protocol is a half-duplex, a single GPIO is used in DA1453x for the external UART. The protocol is the same as for a two-wire UART booting except that the Booter SW need to change the pin direction before sending or receiving information. The bootloader of the DA1453x support a 1-wire UART interface on pin P0_5 or P0_3 which is option(step) 2 or option(step) 3 of the booting sequence. To boot from P0_3, connect the FTDI RX and TX via a 1K resistor and connect the RX side of FTDI to the P0_3 pin.

Hint

The 1K resistor exists in the motherboard, when using it there is no need to do that.

The jumper settings to use the 1-wire UART are as shown in Figure 18 and Figure 19. They are marked as a white box with a red outline. The jumpers are set to enable the 1-wire UART functionality along with SWD but not the Flash. Using flash and 1-wire UART is described in the coming sections.

../_images/Jumper2.svg

Figure 18 Jumper Settings for 1-wire UART on DA14531 DevkitP

../_images/Jumper_5351.svg

Figure 19 Jumper Settings for 1-wire UART on DA1453x DevkitP

Booting on the 1-wire UART using the SmartSnippets™ Toolbox requires the following settings:
  • Select your target from Board tab on top right side of the application:
    ../_images/SmartSnippets.svg

    Figure 20 SmartSnippets™ Toolbox Settings

  • Select P0_5, P0_5, 115200 Bd from Configurator, Board Setup , UART communication and in the boot ROM browse through the binary you want to download to SysRAM as shown in Figure 20
    ../_images/Board_Setup.svg

    Figure 21 Board Setup and Booter

  • Check the logs to confirm the firmware download and now the device will boot from 1-wire UART.

7.1.1. Programming Flash using 1-wire UART

The Flash memory connected over SPI to the DA1453x can be accessed over the 1-wire UART. The description below will explain how to program the firmware into the Flash memory. To boot from SPI Slave using the 1-wire UART, the jumper settings and the board setup are shown in Figure 22.

../_images/Jumper_flash.svg

Figure 22 Jumper Settings 1-wire UART with SPI Flash (Default)

../_images/Jumper_535_flash.svg

Figure 23 Jumper Settings 1-wire UART with SPI Flash (Default) (DA1453x DEvkitP)

../_images/SmartSnippets.svg

Figure 24 UART/SPI Selection

Once you have these configurations, the following steps to connect/read/write/erase are like in Section 6.2.1 . The DA1453x bootloader is capable also of booting from a specific booting path (new SPI pin assignment). We simply need to use the configuration properly by applying it in the OTP header fields. An application can determine by using the OTP header fields which SPI pins the boot ROM should use for booting from external non-volatile memory. Consider the following example:

SPI-CLK: P0_4 SPI-CS: P0_8 SPI-MISO: P0_3 SPI-MOSI: P0_6

The OTP header breakdown on the 0x7F87FC8 and 0x7F87FCC addresses is presented in Section 6.3. On address 0x7F87FC8 the application should program: 0x02FFABAA (1 wire UART)

On address 0x7F87FCC the application should program: 0x03060804

Hint

Boot from Specific SPI Port provides more details about Booting from Specific SPI port.

../_images/otp_header.svg

Figure 25 The OTP Header Burned with New Values

7.2. Booting from 2-wire UART

The bootloader of the DA1453x supports a 2-Wire UART interface on pin P0_0 and pin P0_1. The hardware and software setup are like 1-wire UART except for the jumper settings and board setup as shown in Figure 26 ,:numref:Jumper Settings for 2-wire UART (P0_0 and P0_1) (on DA1453x DevkitP) and Figure 28.

../_images/Jumper_set.svg

Figure 26 Jumper Settings for 2-wire UART (P0_0 and P0_1)

../_images/Jumper_set_535.svg

Figure 27 Jumper Settings for 2-wire UART (P0_0 and P0_1)

The configuration on SmartSnippets™ Toolbox for 2-wire UART is as follow

../_images/2-wire.svg

Figure 28 Board Setup for 2-wire UART

The jumper settings on the motherboard from J1 to the J2 header are as shown in Figure 21. The UTX (of the FTDI chip) is connected using a jumper cable to J2-P20 (P0_0/UART-Tx of the DA1453x) and URX (of the FTDI chip) is connected to J2-P21 (P0_1/UART-Rx of the DA1453x). Using the Booter from the SmartSnippets™Toolbox, download the firmware and the DA1453x will boot from the 2-wire UART as per step 4 of the boot sequence.

7.2.1. Programming Flash using 2-wire UART

The Flash memory connected over SPI to the DA1453x can be accessed over the 2-wire UART. The description below will explain how to program the firmware into the Flash memory. To boot from SPI Slave using the 2-wire UART, the jumper settings and the board setup are shown in Figure 30 and Figure 29 . To boot from SPI Slave using the 2-wire UART needs a modification in the pin configuration due to the reason that the P0_0 is multiplexed between DA1453x-UART Tx and SPI slave MOSI. Due to this reason we modify the pin configuration in the following way as shown below.

../_images/pin.svg

Figure 29 SPI-Flash Pin Configuration on DA14531 DevkitP

../_images/pin_535.svg

Figure 30 SPI-Flash Pin Configuration on DA1453x DevkitP

SPI Flash Pin Config

MOSI (SPI_DO) - P0_5 CS (SPI_EN) - P0_6 MISO (SPI_DI) - P0_3 CLK (SPI_CLK) - P0_4

Configuring DA1453x UART for SPI Flash Access and OTP Burning of Secondary Bootloader

When 2 wire UART (UART_TX = P0_0 and UART_RX= P0_1) is used to access the SPI flash (assuming that the P0_0 is not of any SPI pins), the DA1453x secondary bootloader should be used to boot from a specific booting path (new SPI pin assignment). We simply need to burn it in the OTP.

Simplified SPI Flash Access Using 1-Wire UART (P0_5) on DA1453x

When the 1 wire UART (P0_5) is used to access the SPI flash, the secondary bootloader is no longer needed.

Enhanced SPI Flash Access with 1-Wire UART (P0_5) on DA1453x, Eliminating the Secondary Bootloader Requirement

When the P0_0 is used as one of any SPI pins, the 1 wire UART (P0_5) could be used to access the SPI flash and then the secondary bootloader is no longer needed.

DA1453x Configuration: 1-Wire UART and SPI Integration with OTP Header Setup

When the P0_0 is used as one of the SPI pins, and also as UART_TX the secondary bootloader is no longer needed. You simply need to program the OTP header on the 0x7F87FC8 and 0x7F87FCC addresses, consider for instance the following example:

SPI-CLK: P0_0 SPI-CS: P0_8 SPI-MISO: P0_3 SPI-MOSI: P0_6

On address 0x7F87FC8 the application should program: 0x00FFABAA (2 wire UART) On address 0x7F87FCC the application should program: 0x03060800

../_images/pin.svg

Figure 31 Jumper config 2-wire UART with SPI Flash

Enabling SWD Interface in DA1453x: Application Code Configuration with SYS_CTRL_REG

The SWD interface is disabled when OTP is programmed on DA1453x. It is possible to re-enable SWD in your application code via the configuration script. You need to program 0x1A1 to the SYS_CTRL_REG (P0_2 / P0_10). If the Firmware burned in the OTP has the debugger enabled, then the SWD interface will be enabled from the application itself without explicitly burned the configuration script.

void SystemInit (void)

#endif
{
        SetBits16(SYS_CTRL_REG,DEBUGGER_ENABLE,1);

Refining SWD Interface Reactivation in DA1453x Application Code: A Systematic Approach

For application code mentioning the DEBUGGER_ENABLE bits in SYS_CTRL_REG as just writing 0x1A1 to this register in application code can result in unexpected behavior, especially as this will remap OTP at 0x00000000 when a reset is triggered.

  • To write on this register first on programmer tab choose OTP on left side bar choose Configuration Script:
    ../_images/OTP2.png

    Figure 32 OTP tab

  • Click on the Configuration Script in the table. In the Manage Configuration Script window you will see the following result:
    ../_images/OTP.png

    Figure 33 Configuration Script

  • In Add command of type, you will see a menu of different commands , choose Register Configuration and then click on ADD
    ../_images/OTP4.png

    Figure 34 Register Selection

  • In select of register , type sys_CTRL_REG. Write the value 1A1.
    ../_images/OTP5.png

    Figure 35 Select and write the HEX value