9. Your First DA1469x Application – FreeRTOS_Retarget
9.1. Introduction
The following sections explain how the user can build, program and run a
simple software application called Freertos_retarget
on the ProDK
development board using the SmartSnippets™ DA1469x SDK.
This application is a basis for creating your own applications with FreeRTOS support.
It is a pre-defined project template called freertos_retarget
which is located at <sdk_root_directory>\projects\dk_apps\templates
.
The application is first described, then step by step instructions are given to build and run it.
9.2. Software Architecture
In order to be familiar with building and executing freertos_retarget
project
is better to run it in debug mode first. This is the easiest setup and does
not need any Flash programming prior to executing the binary.
When the application starts running the first thing that is executed is
the Reset_Handler
, which is located in startup > startup_ARMCM0.s
. This
is followed by setting IRQ
priorities and initializing variables.
Next, code execution continues with the main subroutine in file main.c.
Here, the main routine creates the task SysInit
and starts the RTOS scheduler.
From now on the RTOS scheduler is running and it will start the first task which
is SysInit
.
The SysInit
first initializes the clock and the low power clock and sets the
clock dividers for AHB and APB buses. Then retarget is initialized which leads to
initialization of the UART one peripheral. This includes setting up the fifo mode,
dma, baudrate and enabling the communication power domain and the UART one peripheral.
Main routine continues with wakeup configuration. It sets xtal as the clock that is used in wake up and wake up mode to fast wake up.
Last thing done before SysInit
task exits is to create another task
prvTemplateTask
which is the main application task running until the program gets
stopped. The function code implementing this main task is as follows:
static void prvTemplateTask( void *pvParameters )
{
OS_TICK_TIME xNextWakeTime;
static uint32_t test_counter=0;
/* Initialise xNextWakeTime - this only needs to be done once. */
xNextWakeTime = OS_GET_TICK_COUNT();
for ( ;; ) {
/* Place this task in the blocked state until it is time to run again.
The block time is specified in ticks, the constant used converts ticks
to ms. While in the Blocked state this task will not consume any CPU
time. */
vTaskDelayUntil( &xNextWakeTime, mainCOUNTER_FREQUENCY_MS );
test_counter++;
if (test_counter % (1000 / OS_TICKS_2_MS(mainCOUNTER_FREQUENCY_MS)) == 0) {
printf("#");
fflush(stdout);
}
}
}
The software as provided in the SmartSnippets™ DA1469x SDK – once up and running - interacts with a host PC and sends the character ‘#’ via the serial UART interface every 1sec. This can be verified by setting up a terminal application (see Section 6.3.3 for the procedure, with the only difference that now the baud rate must be set to 115200).
9.3. Software Build
This section describes all the steps required to import, build and run this first project.
In the SmartSnippets™ Studio welcome page click on the IDE icon from the Tools tab as shown in Figure 36.
Import the template project
freertos_retarget
from:<sdk_root_directory>\projects\dk_apps\templates\freertos_retarget
into the selected workspace. Press the browse button highlighted in the Resources tab (reference 1) and navigate to the folder which contains the specific project as shown in Figure 37.
In the same way import the
python_scripts
project from:<sdk_root_directory>\utilities\python_scripts
9.3.1. Build the project to run from RAM
The first build to try is a RAM build. This is the simplest one as there is no need to write the code to external QSPI Flash, the debugger will load it directly into RAM from where it can be run. This is not the normal method of development.
Build the project with the Build button and select Debug RAM configuration DA1469x-00-Debug-RAM
as shown in Figure 38.
Once the Debug RAM binary is built, the next step is to start the Debugger using Run > Debug Configurations > SmartBond “SmartSnippets DA1469x SDK via J-Link GDB Server > RAM as shown in Figure 39. As this is a RAM build the debugger will download the binary file via J-Link debugger into the system RAM. To enable this the system RAM is mapped to address 0 by the debugger.
9.3.2. Build the project to run from QSPI Flash
This will be the normal development flow which has three steps: build the code, write it to QSPI Flash and then run it in the debugger.
Build the project pressing the build button and select the Debug QSPI configuration
DA1469x-00-Debug-QSPI
as shown in Figure 40.
The next step is to write the binary file to QSPI Flash. This is done by using a script selected from the
External Tool button. In Figure 41 select program_qspi_jtag
to program the
QSPI Flash memory. (The external tools may not be populated at first use. To populate the External Tool button, press the
External Tools Configuration… button to manually add the menu items.)
Alternatively, use Run > External Tools > program_qspi_jtag.
Finally start the debugger using Run >Debug configurations > Smartbond “SmartSnippets DA1469x SDK” > QSPI and click ‘Debug’ as shown in Figure 42. This will start the debug perspective in SmartSnippets™ and load the symbols for the current project into the debugger.
9.4. Configure SmartSnippets™ to write to Flash
In order to write an image to Flash a configuration must be done first. Press in
Figure 41 the program_qspi_config
to access configuration menu.
Alternatively, use Run > External Tools > program_qspi_config. This will open the window Figure 43
with a summary of the current QSPI configuration and supported device.
Press change to apply a new configuration. The first question has to do with the Product Id
Select DA1469x-00
product family.
Next you will be asked about the Flash configuration. For Pro DK of the DA1469x family select MX25U3235F
.
Finally, you will be asked to insert an address about Active FW image address
and Update FW image address
.
Please keep in both entries the default value 0x2000.
9.5. Running the project in the Debugger
Now that the binary has been loaded to memory (either RAM by debugger or QSPI by script) and the debugger has the symbols for the project loaded it is possible to run project in the debugger.
Start execution of the FreeRTOS retarget project by selecting Resume inside the SmartSnippets™ Run menu or by hitting the play icon as indicated in Figure 46.
The correct functionality of the FreeRTOS retarget project can be checked by noticing in the host PC that target sends the character ‘#’ via the serial UART interface every 1sec.