Default system rand() function is not NIST compliant
ID: LPCBARESDK-765
Status: Open
First reported: 6.0.14.1114
Fixed in: TBD
Description
For the DA14585/586/531: Default system rand() function is not NIST compliant.
Workaround
It is suggested to use the alternative chacha20() function, when true random numbers are required (NIST compliant).