PDM support

ID: LPCBARESDK-693

Status: Open

First reported: 6.0.14.1114

Fixed in: TBD

Description

The PDM driver files in the SDK6.0.14 (in sdkplatformdriverpdm) do not compile. The driver have not been updated to to support the new DMA API introduced in that same release. Some PDM definitions are missing new the new DMA drivers, like the PDM trigger settings.

Workaround

Contact your Dialog representative.