DA14531 IAR Example : Some missing configuration

ID: LPCBARESDK-686

Status: Open

First reported: 6.0.14.1114

Fixed in: TBD

Description

some missing configurations on the IAR project to be able to debug the DA14531 on C level instead of ASM.

Workaround

The workaround of this issue is availbale Here.